STM32H7 Ethernet transmission comes to halt, eventually related to TX queue underflow interrupt?
Hi,
I experience strange behaviour with the just reworked H7 ethernet driver in STM32H725 with LwIP + FreeRTOS environment. A continuous transmission of UDP frames (bursts of 3..4 frames every ~ 50 ms) comes to halt after just a few successful loops. The "heth.gState" changes to HAL_ETH_STATE_BUSY and remains so forever.
Interestingly, I added some lines of debug code that reads the MAC register contents just before calling HAL_ETH_Transmit_IT() in LwIP low_level_output() for later comparison, and the halting didn't occur anymore. The access can be further reduced to a single read access to the MAC MTLRQDR (Offset 0x0D38) and it still runs.. but without that particular register access, output reproducibly halts.
The MTLRQDR register by the way changes from 0 (first read) to 1 (second read) in approximately that moment where the halting otherwise would occur (but that's just an assumption, because reading it changes the behaviour).
Now I have two questions:
- Why does reading that register change anything?
- If there is an actual TX underflow, what might be the cause and what can I do against it?
My code uses the stm32h7xx_hal_eth.c driver and adapted ethernetif.c (from STM32CubeH7/Projects/NUCLEO-H723ZG/Applications/LwIP/LwIP_HTTP_Server_Socket_RTOS)
- https://github.com/STMicroelectronics/STM32CubeH7/pull/195
- https://github.com/STMicroelectronics/stm32h7xx_hal_driver/pull/16
Thanks for your ideas and help in advance!
Kolja