STM32H7 Series - Can semaphore in FreeRTOS be used in USB interrupt handler?
Hi,
I'm using USB mass storage to receive and store the data to external SPI flash ROM. I hope the SPI interface can be using semaphore method, but when I used osSemaphoreWait function in STORAGE_Write_FS function it might cause the device to timeout when the PC starts to receive the data. I'm certain that without semaphore method SPI can be worked for storage data through STORAGE_Write_FS function receive. Suggest using semaphore in interrupt handler?