STM32H7 USB OTG HS: Four highest OTG_HS_DIEPTXF registers mirror the low ones
I am trying to set the FIFO sizes for an application that uses 6 bulk IN endpoints. When I write to OTG_HS_DIEPTXF1, it appears that OTG_HS_DIEPTXF5 takes on the same value. Same for DIEPTXF6 taking on the value of DIEPTXF2, and for DIEPTXF7 taking on the value of DIEPTXF3. Writes to DIEPTXF4, 5, 6, and 7 are ignored.
This is not a compiler/software bug, as I can duplicate it by simply using the memory window in my IDE to modify the registers and see duplicate values appear after the write. I didn't see this in the Errata, so I'm wondering if anyone else has had this issue?
I'm using the OTG_HS peripheral of the STM32H750XBHx with an external PHY attached in HS mode.
(One other note: according to the reference manual, the SVD file currently distributed with STM32CubeIDE has an incorrect address offset for OTG_HS_DIEPTXF3: it should be 0x10C, not 0x11C).