Skip to main content
Visitor II
May 23, 2025
Question

STM32H7 with FreeRTOS – How to Handle Large Library

  • May 23, 2025
  • 1 reply
  • 422 views


Hello,

We are preparing a system based on STM32H7 series with FreeRTOS, and the memory configuration includes:

  • External SDRAM
  • External Serial Flash (QSPI)

We plan to use a large static library (.a) with code and data totaling several megabytes. We have the following questions:

Q1. Handling Large Static Libraries
What is the recommended way to use large .a libraries in STM32 environments?
Are there common approaches to load/execute them from external memory such as SDRAM?

Q2. Dynamic Loading via QSPI Flash and File System
Is it feasible to store the library as a binary file in QSPI Flash (with a file system), then load it into SDRAM at runtime and execute it dynamically ?

We’d appreciate any suggestions, best practices, or examples.

Thanks.

    This topic has been closed for replies.

    1 reply

    ST Employee
    May 28, 2025

    Hello @st-kye

    Q1. Your external SDRAM needs to be properly configured using (FSMC) or FMC for efficient SDRAM access.

    Also, you can directly execute from SDRAM with careful configuration of memory regions, note that this method can introduce latency 

    Q2: yes, for loading you'll probably need DMA to transfer the library from QSPI Flash to SDRAM.