Skip to main content
Visitor II
June 26, 2025
Question

STM32H743 ETH DMA MPU SETTING

  • June 26, 2025
  • 1 reply
  • 405 views

 

Hello everyone, I am using the LWIP protocol stack on an STM32H743.
I'm a bit confused about the MPU configuration here.
I currently have the DMA receive and transmit descriptor addresses set to 0x30040000 and 0x30040100 respectively.
The DMA receive buffer (RxBuff) address is set to 0x30040200.
My configuration is as follows:

HAL_MPU_Disable(); 
MPU_InitStruct.Enable = MPU_REGION_ENABLE; 
MPU_InitStruct.BaseAddress = 0x30040000; 
MPU_InitStruct.Size = MPU_REGION_SIZE_512B;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; 
MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE; 
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE; 
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE; 
MPU_InitStruct.Number = MPU_REGION_NUMBER5; 
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; 
MPU_InitStruct.SubRegionDisable = 0x00; 
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE; 
HAL_MPU_ConfigRegion(&MPU_InitStruct); 
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT); 

MPU_InitStruct.Enable = MPU_REGION_ENABLE; 
MPU_InitStruct.BaseAddress = 0x30040200; 
MPU_InitStruct.Size = MPU_REGION_SIZE_16KB; 
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; 
MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE; 
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE; 
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE; 
MPU_InitStruct.Number = MPU_REGION_NUMBER6; 
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1; 
MPU_InitStruct.SubRegionDisable = 0x00; 
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE; 
HAL_MPU_ConfigRegion(&MPU_InitStruct); 
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
 

The first descriptor configuration at 0x30040000 works without issues.
But after adding the configuration for 0x30040200, I encounter reception problems – specifically DMA transmit timeouts where the OWN bit in the descriptor doesn't change.
Could you please explain why?

    This topic has been closed for replies.

    1 reply

    Super User
    June 26, 2025

    1. Base address of a MPU region must be aligned on the region size, so the definition of your region #6 is invalid (lines 17-18) 

    2. Setting ETH descriptors and buffers as executable has no sense (and probably can involve weird issues related to  so called "speculative execution")

    3. Remove HAL_MPU_Enable() in line 14. Enable MPU only after configuring the last region.

    Maybe there are more issues...