Skip to main content
Graduate II
August 4, 2025
Question

[STM32H743 + FreeRTOS] How to Monitor Raw LWIP Buffers Without Using recv, send, or select APIs

  • August 4, 2025
  • 1 reply
  • 354 views

Hello ST Community,

I’m currently developing on the STM32H743 using STM32CubeIDE, with the following configuration:

  • FreeRTOS v1 (CMSIS v1 style tasks)

  • LWIP stack configured in RAW API mode (not using netconn or socket layers)

  • Network communication is up and running, and TCP/IP works as expected.


Requirement:

I want to monitor or intercept the raw LWIP buffers, especially:

  • RX and TX pbuf contents

  • Packet payloads

  • PCB-level metadata

...but I want to achieve this without using:

  • lwip_recv(), lwip_send()

  • lwip_select() or POSIX socket APIs


Goal:

  • Build a diagnostic/logging mechanism to observe incoming/outgoing TCP/UDP packets

  • Possibly build a lightweight mirror/sniffer on the MCU itself

  • Debug real-time network traffic without affecting application-level task logic


Key Questions:

  1. Can we hook into pbuf_alloc(), pbuf_free(), or similar functions to mirror buffer contents?

  2. Is there a safe and clean way to tap into the LWIP receive/transmit paths at the core level?

  3. Can tcp_input() or eth_input() be instrumented for monitoring without breaking TCP state?

  4. Is there any ST-recommended way to log or clone traffic from the Ethernet interface before it hits the application?


Any guidance, insights, or experience on raw-level packet monitoring inside STM32H7 + CubeMX-generated LWIP would be greatly appreciated.

Looking forward to expert suggestions from the community.

Warm regards,
Jumman 

    This topic has been closed for replies.

    1 reply

    Graduate II
    August 5, 2025

    Dose any one knows about this?