STM32H743 (with Cube 1.40) ethernet MDIO usage for PHY manufacturer SMI interface with custom opcode
I am trying to use the KSZ8863 IC and (as shown in Table 3-9 of its datasheet) it has many configuration options behind a tweaked version of the standard MIIM interface. In particular, the opcode needs to be set to 00.
I have tried the following:
- directly modify ETH->MACMDIOAR directly to set the PA and RDA bits as required by the KSZ8863 Table 3-9 (instead of HAL_ETH_ReadPHYRegister)
- set MACMDIODR to 0
- set the C45E bit of MACMDIOAR (I am not sure about this and if that makes sense for this PHY, but RM0433 says "When Clause 22 PHY is enabled, only Write and Read commands are valid.")
- Set the GOC bits of MACMDIOAR to 00 (despite it being "reserved" according to RM0433)
This results in a garbage reading. I don't at present have a way to probe the MDIO physical line, so any advice about if this should be possible, and other register settings to try, would be very helpful.
EDIT: forgot to mention that HAL_ETH_ReadPHYRegister works fine for reading the standard PHY registers, so the hardware connections seem OK.