STM32H743XI SDMMC1 SD Card - HAL_SD_ERROR_UNSUPPORTED_FEATURE
Hello,
I'm currently facing an issue with a basic project to setup the SDMMC1 peripheral where the function HAL_SD_Init() fails. The issue is happening inside HAL_SD_Init(), in SD_PowerON(), where it always returns HAL_SD_ERROR_UNSUPPORTED_FEATURE.
I'm using a custom board with the STM32H743XI MCU with an external clock of 26MHz and the STM32CubeH7_FW_H7_V1.11.0 package.
Please find below a picture of the STM32CubeMX Clock configuration:

Here is the code that setup the clock:
void hw_port_clock_init(void)
{
hw_clock_system_clock_init();
hw_clock_init_peripheral_clocks();
}
static void hw_clock_system_clock_init(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = { 0 };
RCC_ClkInitTypeDef RCC_ClkInitStruct = { 0 };
// Supply configuration update enable
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
// Configure the main internal regulator output voltage
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY))
{
}
__HAL_RCC_SYSCFG_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY))
{
}
// Initializes the RCC Oscillators according to the specified parameters in the
RCC_OscInitTypeDef structure.
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 13;
RCC_OscInitStruct.PLL.PLLN = 480;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 24;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_1;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
assert_param(HAL_RCC_OscConfig(&RCC_OscInitStruct) == HAL_OK);
// Initializes the CPU, AHB and APB buses clocks
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_PCLK1 |
RCC_CLOCKTYPE_PCLK2 | RCC_CLOCKTYPE_D3PCLK1 |
RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
assert_param(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) == HAL_OK);
}
static void hw_clock_init_peripheral_clocks(void)
{
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = { 0 };
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SDMMC;
PeriphClkInitStruct.SdmmcClockSelection = RCC_SDMMCCLKSOURCE_PLL;
assert_param(HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) == HAL_OK);
// Enable GPIOs clock
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOF_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
// Enable SDIO clock
__HAL_RCC_SDMMC1_CLK_ENABLE();
}Ans here is the SDMMC1 init code (4bits wide bus):
void hw_port_sd_init(void)
{
/** SDMMC1 GPIO Configuration
PC8 ------> SDMMC1_D0
PC9 ------> SDMMC1_D1
PC10 ------> SDMMC1_D2
PC11 ------> SDMMC1_D3
PC12 ------> SDMMC1_CK
PD2 ------> SDMMC1_CMD
*/
GPIO_InitTypeDef gpio_init_structure = { 0 };
gpio_init_structure.Pin = GPIO_MICROSD_D0_PIN | GPIO_MICROSD_D1_PIN | GPIO_MICROSD_D2_PIN |
GPIO_MICROSD_D3_PIN | GPIO_MICROSD_CLK_PIN;
gpio_init_structure.Mode = GPIO_MODE_AF_PP;
gpio_init_structure.Pull = GPIO_NOPULL;
gpio_init_structure.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
gpio_init_structure.Alternate = GPIO_AF12_SDIO1;
HAL_GPIO_Init(GPIOC, &gpio_init_structure);
gpio_init_structure.Pin = GPIO_MICROSD_CMD_PIN;
gpio_init_structure.Mode = GPIO_MODE_AF_PP;
gpio_init_structure.Pull = GPIO_NOPULL;
gpio_init_structure.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
gpio_init_structure.Alternate = GPIO_MICROSD_CMD_AF;
HAL_GPIO_Init(GPIO_MICROSD_CMD_PORT, &gpio_init_structure);
__HAL_RCC_SDMMC1_FORCE_RESET();
__HAL_RCC_SDMMC1_RELEASE_RESET();
g_sd_handle.Instance = SDMMC1;
g_sd_handle.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;
g_sd_handle.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
g_sd_handle.Init.BusWide = SDMMC_BUS_WIDE_4B;
g_sd_handle.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;
g_sd_handle.Init.ClockDiv = 0;
assert_param(HAL_SD_Init(&g_sd_handle) == HAL_OK);
// NVIC configuration for SDMMC1 interrupt
HAL_NVIC_SetPriority(SDMMC1_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(SDMMC1_IRQn);
}The parameter USE_SD_TRANSCEIVER from stm32h7xx_hal_conf.h is set to 0.
Does anyone experienced this issue before ? Any help would be appreciated.
Many Thanks!
LB