STM32H743ZI2 with USB OTG MSC
Hello,
I have bought myself the STM32H743 Nucleo.
Am trying to explore the environment and learn the working of parts and functions of the board.
The board comes with two on-Board USB Ports. One for the ST-Link and the other is to be used as a user USB port.
I am attempting to connect a USB mass storage device, say a pen drive, through the user USB provided within the board and access it through FATFS.
I need to create a csv file inside the hard disk and write the Analog Input values to the USB Drive.
What I have already tried is listed below :
- I have gone through the Mass storage code for NUCLEO-F446ZE.
- Gone through the User manual tutorial.
- Even gone through the USB tutorial by STMicroelectronics but non of them worked.
I haven't succeeded yet and i now seek help on how this can be implemented.
What should be my approach for implementing this functionality.
Is there any example to better understand how to implement this.?
I would appreciate any kind of input from you.
Looking forward to helpful responses from the community.
Thank you.