Skip to main content
Visitor II
June 8, 2021
Solved

STM32H745 Disco example with eMMC + FatFs not working (FR_DISK_ERR).

  • June 8, 2021
  • 4 replies
  • 2009 views

Hi,

I try to run "FatFs_Shared_Device" example which supposed to demonstrate FatFs and eMMC.

I keep getting FR_DISK_ERR.

Has anyone ever encountered this issue?

I understood it supposed to work without any modification to the example.

Thanks guys

    This topic has been closed for replies.
    Best answer by Walid ZRELLI

    Hello @ABen .1​ ,

    Your issue has been confirmed and tracked internally for resolution. I will keep you posted on updates.

    Alternatively, As a workaround for the faced issue you can use the attached HAL SDMMC driver files to replace the ones in your package.

    Thanks for your contribution.

    BeST Regards,

    Walid

    4 replies

    Visitor II
    June 9, 2021

    Hello @ABen .1​ ,

    Welcome to our ST Community :)

    Can you please provide the version of the package used?

    Thanks in advance.

    BeST Regards,

    Walid

    ABen .1Author
    Visitor II
    June 9, 2021

    Sure.

    STM32Cube_FW_H7_V1.9.0

    Thanks

    Graduate II
    June 9, 2021

    I've had the examples working in the past. ​The eMMC needs formatting as I recall, but that would give a different error.

    Visitor II
    August 22, 2023

    Do you have the example code for stm32f4 with eMMC(iNAND 7250 SD) in 4-bits? 

    ABen .1Author
    Visitor II
    June 9, 2021

    Yeah you are right, the eMMC need to be formatted. I get the error "FR_DISK_ERR" when I try to create a partition using "f_mkfs". I also tried to "f_mount" but getting the same error.

    The board is new and the example downloaded from STM32CubeMX.

    Did this exact example work for you @Community member​ ?

    Thanks!

    Visitor II
    June 9, 2021

    Hello @ABen .1​ ,

    Your issue has been confirmed and tracked internally for resolution. I will keep you posted on updates.

    Alternatively, As a workaround for the faced issue you can use the attached HAL SDMMC driver files to replace the ones in your package.

    Thanks for your contribution.

    BeST Regards,

    Walid

    Visitor II
    July 8, 2022

    Is this issue fixed or still existing ?

    I have ordered 1 unit of the STM32H745I-DISCO and my application include FreeRTOS and FATfs