Skip to main content
Visitor II
January 2, 2025
Solved

STM32h745i-DISCO USB with MMC windows was unable to complete the format

  • January 2, 2025
  • 1 reply
  • 712 views

Hi, 

We are working on MMC with USB on the STM32H745I-Disco board but are unable to format the disk. 

using STM32CubeIDE version is  1.16.1

System Clock Configuration

  • HSE Clock Source
    • CM7 Core: 400 MHz
    • CM4 Core: 200 MHz
  • USB Frequency
    • RC48 Clock: 48 MHz

SDMMC CLK

sivani_1-1735819714232.png

 

RCC

sivani_0-1735819631276.png

SDMMC 

sivani_2-1735819814038.png  

sivani_3-1735819843558.png 

sivani_4-1735819869605.png

 

USB_OTG_FS configuration

sivani_5-1735819920330.png

in middle firmware

sivani_6-1735819984456.png

All these configurations were applied in the CM7 core.

And the location D:\ Mass_storage\CM7\USB_DEVICE\App\usbd_storage_if.c  we added  below function

 

int8_t STORAGE_GetCapacity_FS(uint8_t lun, uint32_t *block_num, uint16_t *block_size)

{

 /* USER CODE BEGIN 3 */

// UNUSED(lun);

// *block_num = STORAGE_BLK_NBR;

// *block_size = STORAGE_BLK_SIZ;

 HAL_MMC_CardInfoTypeDef hmmcInfo;

 if(HAL_MMC_GetCardInfo(&hmmc1, &hmmcInfo) != HAL_OK)

 { return (USBD_FAIL);

 }

 *block_num = hmmcInfo.LogBlockNbr - 1;

 *block_size = hmmcInfo.LogBlockSize;

 return (USBD_OK);

 /* USER CODE END 3 */ 

 } 

 

When we attempt to format the disk from the host system (e.g., Windows), the operation fails with an error

sivani_7-1735820127174.png

 

sivani_8-1735820204618.png 

 

After that in same location .c  file  we added read and write function

 

int8_t STORAGE_Read_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len)

{

 /* USER CODE BEGIN 6 */

 // UNUSED(lun);

 // UNUSED(buf);

// UNUSED(blk_addr);

// UNUSED(blk_len);

 if(HAL_MMC_ReadBlocks(&hmmc1, buf, blk_addr, blk_len, HAL_MAX_DELAY) != HAL_OK)

 {

 return (USBD_FAIL);

// }

 uint32_t timestart = 100000;

 while ((HAL_MMC_GetCardState(&hmmc1) != HAL_MMC_CARD_TRANSFER))

 {

 if ((HAL_GetTick() - timestart) >= SDMMC_DATATIMEOUT)

 {

 return (USBD_FAIL);

 }

 }

return (USBD_OK);

 /* USER CODE END 6 */

}

int8_t STORAGE_Write_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len)

{

 /* USER CODE BEGIN 7 */

 //UNUSED(lun);

 //UNUSED(buf);

 // UNUSED(blk_addr);

 //UNUSED(blk_len);

 if(HAL_MMC_WriteBlocks(&hmmc1, buf, blk_addr, blk_len, HAL_MAX_DELAY) != HAL_OK)

 {

 return (USBD_FAIL);

 }

 uint32_t timestart = 100000;

 while ((HAL_MMC_GetCardState(&hmmc1) != HAL_MMC_CARD_TRANSFER))

 {

 if ((HAL_GetTick() - timestart) >= SDMMC_DATATIMEOUT)

 {

 return (USBD_FAIL);

 }

 }

return (USBD_OK);

 /* USER CODE END 7 */

} 

 

If we added these two function the disk not showing the PC we are getting like this

sivani_9-1735822863667.png

 

Please provide a solution for this issue. I have also attached the relevant firmware configurations for reference.

    This topic has been closed for replies.
    Best answer by FBL

    Hi @sivani 


    If still having the same issue, update latest version of CubeMX and Cube FW H7.

    Changing features involves modifying the USB device descriptor. Each time we change the device descriptor, we may need to reinstall the USB device : uninstall the USB device from the Windows Device Manager and re-plug the USB cable. During this operation, the USB host keeps new information in its registry. Also, changing PID can solve such issue.

    1 reply

    FBLAnswer
    Technical Moderator
    May 9, 2025

    Hi @sivani 


    If still having the same issue, update latest version of CubeMX and Cube FW H7.

    Changing features involves modifying the USB device descriptor. Each time we change the device descriptor, we may need to reinstall the USB device : uninstall the USB device from the Windows Device Manager and re-plug the USB cable. During this operation, the USB host keeps new information in its registry. Also, changing PID can solve such issue.