Skip to main content
Visitor II
March 5, 2020
Question

STM32H747_DISCO board cannot read Audio Data(MP34DT05TR Mic) based on DFSDM

  • March 5, 2020
  • 1 reply
  • 966 views

Board: STM32H747I-DISO

SDK: STM32Cube_FW_H7_V1.6.0

Pin: PD3(CLK), PC7(DATAIN3)

Problem: Filter->DMA bufer OK. HAL_DFSDM_FilterRegConvCpltCallback and HAL_DFSDM_FilterRegConvHalfCpltCallback function enter normally, but the data is wrong(always the same number). 

I monitor the DFSDM registers, the RDATAR register no change.

0690X00000DYmBMQA1.png

0690X00000DYmBqQAL.png

Head Code

/* DFSDM Configuration defines */
#define AUDIO_DFSDMx_RIGHT_CHANNEL DFSDM_CHANNEL_2
#define AUDIO_DFSDMx_LEFT_CHANNEL DFSDM_CHANNEL_3
 
#define AUDIO_DFSDMx_LEFT_FILTER DFSDM1_Filter0
#define AUDIO_DFSDMx_RIGHT_FILTER DFSDM1_Filter1
 
 
#define AUDIO_DFSDMx_CLK_ENABLE() __HAL_RCC_DFSDM1_CLK_ENABLE()
#define AUDIO_DFSDMx_CKOUT_PIN GPIO_PIN_3
#define AUDIO_DFSDMx_CKOUT_DMIC_GPIO_PORT GPIOD
#define AUDIO_DFSDMx_CKOUT_AF GPIO_AF3_DFSDM1
#define AUDIO_DFSDMx_CKOUT_DMIC_GPIO_CLK_ENABLE() __HAL_RCC_GPIOD_CLK_ENABLE()
 
 
#define AUDIO_DFSDMx_DMIC_DATIN_PIN GPIO_PIN_7
#define AUDIO_DFSDMx_DMIC_DATIN_GPIO_PORT GPIOC
#define AUDIO_DFSDMx_DMIC_DATIN_AF GPIO_AF4_DFSDM1
#define AUDIO_DFSDMx_DMIC_DATIN_GPIO_CLK_ENABLE() __HAL_RCC_GPIOC_CLK_ENABLE()
 
/* DFSDM DMA Right and Left channels definitions */
#define AUDIO_DFSDMx_DMAx_CLK_ENABLE() __HAL_RCC_DMA2_CLK_ENABLE()
 
#define AUDIO_DFSDMx_DMAx_LEFT_REQUEST DMA_REQUEST_DFSDM1_FLT0
#define AUDIO_DFSDMx_DMAx_RIGHT_REQUEST DMA_REQUEST_DFSDM1_FLT1
 
#define AUDIO_DFSDMx_DMAx_PERIPH_DATA_SIZE DMA_PDATAALIGN_WORD
#define AUDIO_DFSDMx_DMAx_MEM_DATA_SIZE DMA_MDATAALIGN_WORD
 
#define AUDIO_DFSDMx_DMAx_LEFT_STREAM DMA2_Stream3
#define AUDIO_DFSDMx_DMAx_LEFT_IRQ DMA2_Stream3_IRQn 
#define AUDIO_DFSDMx_DMAx_LEFT_IRQHandler DMA2_Stream3_IRQHandler
 
#define AUDIO_DFSDMx_DMAx_RIGHT_STREAM DMA2_Stream2
#define AUDIO_DFSDMx_DMAx_RIGHT_IRQ DMA2_Stream2_IRQn
#define AUDIO_DFSDMx_DMAx_RIGHT_IRQHandler DMA2_Stream2_IRQHandler
 
/* Select the interrupt preemption priority and subpriority for the DMA interrupt */
#define AUDIO_IRQ_PREPRIO ((uint32_t)0x0E)
 
 
 

Source Code

static void DFSDM_Init(void)
{
 /* Initialize channel 1 (left channel)*/
 __HAL_DFSDM_CHANNEL_RESET_HANDLE_STATE(&DfsdmLeftChannelHandle);
 DfsdmLeftChannelHandle.Instance = DFSDM1_Channel3;
 DfsdmLeftChannelHandle.Init.OutputClock.Activation = ENABLE;
 DfsdmLeftChannelHandle.Init.OutputClock.Selection = DFSDM_CHANNEL_OUTPUT_CLOCK_AUDIO;
 DfsdmLeftChannelHandle.Init.OutputClock.Divider = 24; /* 49.142MHz/24 = 2.047MHz */
 DfsdmLeftChannelHandle.Init.Input.Multiplexer = DFSDM_CHANNEL_EXTERNAL_INPUTS;
 DfsdmLeftChannelHandle.Init.Input.DataPacking = DFSDM_CHANNEL_STANDARD_MODE; /* N.U. */
 DfsdmLeftChannelHandle.Init.Input.Pins = DFSDM_CHANNEL_SAME_CHANNEL_PINS;
 DfsdmLeftChannelHandle.Init.SerialInterface.Type = DFSDM_CHANNEL_SPI_RISING;
 DfsdmLeftChannelHandle.Init.SerialInterface.SpiClock = DFSDM_CHANNEL_SPI_CLOCK_INTERNAL;
 DfsdmLeftChannelHandle.Init.Awd.FilterOrder = DFSDM_CHANNEL_FASTSINC_ORDER; /* N.U. */
 DfsdmLeftChannelHandle.Init.Awd.Oversampling = 10; /* N.U. */
 DfsdmLeftChannelHandle.Init.Offset = 0;
 DfsdmLeftChannelHandle.Init.RightBitShift = 3;
 if (HAL_OK != HAL_DFSDM_ChannelInit(&DfsdmLeftChannelHandle))
 {
 Error_Handler();
 }
 
 /* Initialize channel 0 (right channel)*/
 __HAL_DFSDM_CHANNEL_RESET_HANDLE_STATE(&DfsdmRightChannelHandle);
 DfsdmRightChannelHandle.Instance = DFSDM1_Channel2;
 DfsdmRightChannelHandle.Init.OutputClock.Activation = ENABLE;
 DfsdmRightChannelHandle.Init.OutputClock.Selection = DFSDM_CHANNEL_OUTPUT_CLOCK_AUDIO;
 DfsdmRightChannelHandle.Init.OutputClock.Divider = 24; /* 49.142MHz/24 = 2.047MHz */
 DfsdmRightChannelHandle.Init.Input.Multiplexer = DFSDM_CHANNEL_EXTERNAL_INPUTS;
 DfsdmRightChannelHandle.Init.Input.DataPacking = DFSDM_CHANNEL_STANDARD_MODE; /* N.U. */
 DfsdmRightChannelHandle.Init.Input.Pins = DFSDM_CHANNEL_FOLLOWING_CHANNEL_PINS;
 DfsdmRightChannelHandle.Init.SerialInterface.Type = DFSDM_CHANNEL_SPI_FALLING;
 DfsdmRightChannelHandle.Init.SerialInterface.SpiClock = DFSDM_CHANNEL_SPI_CLOCK_INTERNAL;
 DfsdmRightChannelHandle.Init.Awd.FilterOrder = DFSDM_CHANNEL_FASTSINC_ORDER; /* N.U. */
 DfsdmRightChannelHandle.Init.Awd.Oversampling = 10; /* N.U. */
 DfsdmRightChannelHandle.Init.Offset = 0;
 DfsdmRightChannelHandle.Init.RightBitShift = 3;
 if (HAL_OK != HAL_DFSDM_ChannelInit(&DfsdmRightChannelHandle))
 {
 Error_Handler();
 }
 
 /* Initialize filter 0 (left channel) */
 __HAL_DFSDM_FILTER_RESET_HANDLE_STATE(&DfsdmLeftFilterHandle);
 DfsdmLeftFilterHandle.Instance = DFSDM1_Filter0;
 DfsdmLeftFilterHandle.Init.RegularParam.Trigger = DFSDM_FILTER_SW_TRIGGER;
 DfsdmLeftFilterHandle.Init.RegularParam.FastMode = ENABLE;
 DfsdmLeftFilterHandle.Init.RegularParam.DmaMode = ENABLE;
 DfsdmLeftFilterHandle.Init.InjectedParam.Trigger = DFSDM_FILTER_SW_TRIGGER; /* N.U. */
 DfsdmLeftFilterHandle.Init.InjectedParam.ScanMode = ENABLE; /* N.U. */
 DfsdmLeftFilterHandle.Init.InjectedParam.DmaMode = DISABLE; /* N.U. */
 DfsdmLeftFilterHandle.Init.InjectedParam.ExtTrigger = DFSDM_FILTER_EXT_TRIG_TIM1_TRGO; /* N.U. */
 DfsdmLeftFilterHandle.Init.InjectedParam.ExtTriggerEdge = DFSDM_FILTER_EXT_TRIG_RISING_EDGE; /* N.U. */
 DfsdmLeftFilterHandle.Init.FilterParam.SincOrder = DFSDM_FILTER_SINC3_ORDER;
 DfsdmLeftFilterHandle.Init.FilterParam.Oversampling = 128; /* 49.142MHz/(24*128) = 16KHz */
 DfsdmLeftFilterHandle.Init.FilterParam.IntOversampling = 1;
 if (HAL_OK != HAL_DFSDM_FilterInit(&DfsdmLeftFilterHandle))
 {
 Error_Handler();
 }
 
 /* Initialize filter 1 (right channel) */
 __HAL_DFSDM_FILTER_RESET_HANDLE_STATE(&DfsdmRightFilterHandle);
 DfsdmRightFilterHandle.Instance = DFSDM1_Filter1;
 DfsdmRightFilterHandle.Init.RegularParam.Trigger = DFSDM_FILTER_SYNC_TRIGGER;
 DfsdmRightFilterHandle.Init.RegularParam.FastMode = ENABLE;
 DfsdmRightFilterHandle.Init.RegularParam.DmaMode = ENABLE;
 DfsdmRightFilterHandle.Init.InjectedParam.Trigger = DFSDM_FILTER_SW_TRIGGER; /* N.U. */
 DfsdmRightFilterHandle.Init.InjectedParam.ScanMode = ENABLE; /* N.U. */
 DfsdmRightFilterHandle.Init.InjectedParam.DmaMode = DISABLE; /* N.U. */
 DfsdmRightFilterHandle.Init.InjectedParam.ExtTrigger = DFSDM_FILTER_EXT_TRIG_TIM1_TRGO; /* N.U. */
 DfsdmRightFilterHandle.Init.InjectedParam.ExtTriggerEdge = DFSDM_FILTER_EXT_TRIG_RISING_EDGE; /* N.U. */
 DfsdmRightFilterHandle.Init.FilterParam.SincOrder = DFSDM_FILTER_SINC3_ORDER;
 DfsdmRightFilterHandle.Init.FilterParam.Oversampling = 128; /* 49.142MHz/(24*128) = 16KHz */
 DfsdmRightFilterHandle.Init.FilterParam.IntOversampling = 1;
 if (HAL_OK != HAL_DFSDM_FilterInit(&DfsdmRightFilterHandle))
 {
 Error_Handler();
 }
 
 /* Configure regular channel and continuous mode for filter 0 (left channel) */
 if (HAL_OK != HAL_DFSDM_FilterConfigRegChannel(&DfsdmLeftFilterHandle, DFSDM_CHANNEL_3, DFSDM_CONTINUOUS_CONV_ON))
 {
 Error_Handler();
 }
 
 /* Configure regular channel and continuous mode for filter 1 (right channel) */
 if (HAL_OK != HAL_DFSDM_FilterConfigRegChannel(&DfsdmRightFilterHandle, DFSDM_CHANNEL_2, DFSDM_CONTINUOUS_CONV_ON))
 {
 Error_Handler();
 }
}

    This topic has been closed for replies.

    1 reply

    Visitor II
    July 7, 2020

    Hello, @zjiaz.1​ ,

    Do you figure out this issue? I face the same problem and i see around that many others have troubles but there is no answer for now.

    I layed my work on stm32h747-eval DFSDM example and i tailored it for my stm32h747i-disco but my left and rightbuf always be filled by same value -16777216 and so when they in SaturaLH the play buf is filled by -32768. So I supposed that it about error configuration on DFSDM init. Is someone can please bring us response?

    Thanks,