STM32H747: SAI with DMA on M7 core causes gaps in I2S stream, works fine on M4
Hi everyone,
I'm working on a project based on the following STM32H7 LwIP example:
https://github.com/stm32-hotspot/STM32H7-LwIP-Examples/tree/main/STM32H747_Disco_M7_ETH
In addition to the Ethernet functionality, I’ve enabled the SAI peripheral with DMA to transmit audio via I2S. I’ve noticed a problem:
When I run the SAI with DMA on the Cortex-M7 core using FreeRTOS, the audio stream contains gaps or dropouts.
However, when I move the exact same SAI/DMA initialization and logic to the Cortex-M4 core, the audio output is perfect with no gaps.
Has anyone experienced similar issues when using DMA for audio on the M7 core with FreeRTOS?
Any suggestions would be greatly appreciated.
Thanks in advance!
TG808