Skip to main content
Graduate II
May 9, 2025
Question

STM32H750 - Watchdog Timer Processing (Handy hint)

  • May 9, 2025
  • 1 reply
  • 538 views

Hi All,

I had the need to use the independent watchdog timer and rather than a straight reset of the system I wished to put the system into a fault mode. You can do this by examining the RCC control and status register (CSR) viz:

 

int main(void)
{
 /* MCU Configuration--------------------------------------------------------*/
	/* TODO: */

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* Configure the system clock */
 SystemClock_Config();

 MX_USART2_UART_Init();
 checkIWDG();

#if(IWDG_ENABLE == 1)
void checkIWDG(void)
{
	if(RCC->CSR & RCC_CSR_IWDGRSTF)
	{
 /*** FAULT MODE ***/
		/* The IWDG has reset the system */
		printf("IWDG Reset\n\r");
		/* Run fans flat out */
		GPIO_InitTypeDef GPIO_InitStruct = {0};

		__HAL_RCC_GPIOA_CLK_ENABLE();

		/*Configure GPIO pins : PA9_FAN1_POWER_Pin PA10_FAN2_POWER_Pin */
		GPIO_InitStruct.Pin = PA9_FAN1_POWER_Pin|PA10_FAN2_POWER_Pin|PA11_TEST_OUTPUT_Pin|PA6_TIM3_CH1_FAN1_SPEED_DEMAND1_Pin|PA7_TIM3_CH2_FAN1_SPEED_DEMAND2_Pin;
		GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
		GPIO_InitStruct.Pull = GPIO_NOPULL;
		GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
		HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

		/* Set the GPIO Pins */
		HAL_GPIO_WritePin(PA10_FAN2_POWER_GPIO_Port, PA10_FAN2_POWER_Pin, GPIO_PIN_SET);
		HAL_GPIO_WritePin(PA9_FAN1_POWER_GPIO_Port, PA9_FAN1_POWER_Pin, GPIO_PIN_SET);
		HAL_GPIO_WritePin(PA6_TIM3_CH1_FAN1_SPEED_DEMAND1_GPIO_Port, PA6_TIM3_CH1_FAN1_SPEED_DEMAND1_Pin, GPIO_PIN_RESET);
		HAL_GPIO_WritePin(PA7_TIM3_CH2_FAN1_SPEED_DEMAND2_GPIO_Port, PA7_TIM3_CH2_FAN1_SPEED_DEMAND2_Pin, GPIO_PIN_RESET);

		while(1)
		{
			printf("Watchdog Timed out\n\r");
			HAL_IWDG_Refresh(&hiwdg);
			HAL_Delay(20000);
		}
	}
	else
	{
 /*** OPERATING MODE (No Fault) ***/
		printf("No IWDG Reset\n\r");
	}
}
#endif

 

In my example I cam controlling a couple of computer fans each with a relay and a demand signal.  If the fan algorithm fails for any reason after 32 seconds the watchdog will reset the cpu and the RCC_CSR_IWDGRSTF gets set.  This forces places the system into a "fans full on mode" and it loops continuously in this mode.

 

When debugging if the RCC_CSR_IWDGRSTF gets set you can only clear it by a power down reset.  Restarting the debugger which uses the reset pin on the cpu will not clear the RCC_CSR_IWDGRSTF bit.

 

Note that if you wish to use the virtual com port to print messages you will need to initialise the uart before checking the RCC_CSR_IWDGRSTF.

Hope someone finds this useful.

 

Regards

Rob

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    May 23, 2025

    Hello @Garnett.Robert 

    It seems that you missed configuring and starting the IWDG in your project before performing the refresh.

    Please refer to the IWDG_WindowMode projects for typical usage of the IWDG peripheral. This reference project is available within the STM32CubeH7 package on st web site.

    Here below the link to download the package:

    STM32CubeH7 - STM32Cube MCU Package for STM32H7 series (HAL, Low-Layer APIs and CMSIS, USB, TCP/IP, File system, RTOS, Graphic - and examples running on ST boards) - STMicroelectronics

    With Regards