Skip to main content
Visitor II
January 25, 2023
Question

STM32H750XB USB I/Fs

  • January 25, 2023
  • 1 reply
  • 675 views

Hi

On STM32H750XB datasheet it says 2 x USBUSB OTG interfaces (1FS, 1HS/FS) .

I configured the 1st port as FS, and the 2nd port as HS which connectd to external PHY (internal FS phy disabled) .

I want to confirm that if the 2 ports can be used at different speed (1 as FS and 1 as HS) at the same time just for sure.

Thanks

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    January 25, 2023

    Hello @YHail.1​ and welcome to the Community :)

    I confirm that both instances should work at the same time.

    When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

    Imen