STM32H753 Ethernet DMAMR register fails to reset when SWR bit is set
While setting up Ethernet connectivity on STM32H753, the HAL layer exited with HAL error during initialization. I found out that the SET_BIT(heth->Instance->DMAMR, ETH_DMAMR_SWR); fails to reset the register and the initialization exits with HAL error on timeout. I am using DP83848 as Ethernet PHY. I was able to verify that the link state is 100-Mbps Full Duplex and 25MHz clock is available as TX_CLK and RX_CLK. The PHY is used in MII mode.