STM32H753 Ethernet using FreeRTOS and lwIP - continued...
Greetings,
trying to get a setup with stm32h753 running FreeRTOS and LwIP. One attempt in this journey was to take the example: How to create project for STM32H7 with Ethernet an... - STMicroelectronics Community
Using the example code, I see one issue with the core lock - if the breakpoint in ethernetif.c line 987 is enabled I see the code suspends in places one would not expect it to suspend such as:

If I disable the breakpoint, ping works ok.
However even with this example the code quite often (if not always) gets stuck to Ethernet output, it seems that a packet comes down to ethernet low_level_output function, but never gets out to the cable. Suspecting it is a DMA issue, but had no luck locating the issue yet. Any ideas?
Thanks!