STM32H755 – End-of-Frame Detection Fails Only with EventFlags, Works with Polling
Hello ST Team,
I am using an STM32H755ZIT6 where CM7 handles a high-speed Quad-SPI flash interface with 100Mhz and UART communication with flow control 115200 baud.
The same firmware runs on two hardware revisions:
Revision V2: Works perfectly
Revision V3: Same firmware → occasional failure in UART frame processing
The QSPI itself receives data correctly (verified with CRC), but the “end of frame” indication is occasionally not processed.
Observed Firmware Behavior
1. Using RTOS Event Flags (original implementation)
In the UART receive callback, when “end of frame” (EOF) is detected, we set an RTOS event flag:
osEventFlagsSet(dataReceiveEvent, DataReceived);Problem on V3:
Sometimes the event flag is not triggered
Even though all received bytes are correct
CRC validation passes
The callback executes, but the main task does not wake
This leads to missed packets even though the data is fully received.
2. Switching to Polling Loop (temporary workaround)
We replaced the RTOS event flag with a simple polling mechanism inside the processing task:
while(1)
{
if(osMessageQueueGet(...) == osOK)
process();
osDelay(10);
}With this change:
V3 hardware works consistently
No EOF detection failures
No lost frames
V2 continues to work as usual
This confirms the raw UART data is always correct — only the timing window of the RTOS wake-up is sensitive.
3. Interpretation (What I need ST guidance on)
It appears that:
The UART ISR + RTOS event-flag + context switching timing is borderline in some conditions
Minor timing jitter causes occasional missed RTOS event wakeups
Polling hides this issue because it does not depend on a precise timing window
4. Questions for ST
Are there known conditions where CMSIS-RTOS2 EventFlags used inside UART RX callbacks can be missed due to timing jitter or interrupt priority interactions?
Is there any recommendation on:
Minimum ISR execution time
Maximum recommended operations inside UART RX callback
Priority level requirements for tasks waiting on EventFlags
Does ST recommend using:
Ring buffer + task polling
Direct-to-queue from ISR
Stream buffer
Event flags
for continuous, critical UART communication?
Any known errata for STM32H7 regarding:
EventFlags not waking tasks
Interrupt latency
Missed wakeups under high-load conditions
5. Summary
Data reception is always correct
CRC is valid
Only the RTOS event flag wake-up occasionally fails
Polling solves the problem
Need guidance on recommended ISR → task signaling method for STM32H7
Thank you in advance.