STM32H755 with Precision Time Protocol.
Hello all,
I am learning to implement a bare-minimal code that let PTP(OC, slave mode) works with STM32H755(Nucleo-H755ZI-Q with FreeRTOS). I have read RM0399, UM2217 as well as stm32h7xx_hal_eth.c with corresponding chapters. And here is the first draft I have done: https://codefile.io/f/vny07A1hYW. In this implementation only PTP-over-Ethernet (PTPv2) will be considered.
So basic ideas are:
+ "DataQ_PTP_Init" implements RM0399 §61.9.9 "Initializing the System time generation". This function will be called with ETH_Init(). As well as when network cable status is changed(connected).
+ "DataQ_PTP_DeInit" will be called when e.g. network cable is disconnected.
+ "DataQ_PTP_SysTime_Fine_Correction" implements RM0399 Page 3037 "System time correction" algorithm, with Fine-Correction only.
+ "DataQ_PTP_TSI_ISR" will verify Addend Register, has been updated correctly. By referencing RM0399 Page 3037 "System time correction" algorithm step 3-8. (When TSI interrupt is triggered.)
+ "DataQ_PTP_Rx_ISR" will update Master_Sync_Time and Slave_Clock_Time, used by Fine-Correction algorithm. (When Rx interrupt is triggered.)
My questions:
+ Could experts here help to identify logical / implementation errors?
+ From RM0399 Page 3037 "System time correction" Step 6. Should be "bit 3/TSUPDT" instead of "bit 4" shown on the document?
+ Why "System time correction" algorithm, step 8, says "reprogram ETH_MACTSAR with old value"? Should be the value updated from the next round of algorithm?
+ How "t3" and "t4" being used in this algorithm, with illustrated in Figure 831 from RM0399?
+ Does "Fine-correction" could be suitable used for initialization e.g. huge time differences between Slave and Master? I am thinking it will take long time elapsed till clock converged.
+ Seems the variable "Master_To_Slave_Delay" never got updated based on "System time correction" algorithm.
+ How to determine the value written to "MACPPSTTSR" and "MACPPSTTNR", from step 4 of "System time correction".
Sorry to say but this is the first time I touched PTP. So for sure there might be some misunderstanding or "guess-work"....
Big Thanks for your kindly help!
Best regards,