Skip to main content
Visitor II
August 21, 2024
Solved

STM32H757 SDMMC1 only works with M7 core

  • August 21, 2024
  • 1 reply
  • 1507 views

Hello,

I am using a Riverdi RVT101HVSNWC00 board (with STM32H757) for a product that needs a display, interfaces to devices, and writes data to a microSD card. After communicating with Riverdi, I gathered the correct SDMMC1 configuration to make the peripheral work and allow the Cortex-M7 core to write data to the filesystem on the SD card. M7 is completely functional with the SD card. However, the software architecture I would like to implement requires that the Cortex-M4 core be responsible for the SD card. I cannot get the M4 to even initialize the SDMMC1 peripheral no matter what I do.

I have SDMMC1 enabled for only the M4 core in CubeMX, with the correct peripheral, DMA, and FatFs configuration. When M4 calls MX_SDMMC1_SD_Init(), execution eventually comes to HAL_SD_InitCard() in stm32h7xx_hal_sd.c. This then calls HAL_RCCEx_GetPeriphCLKFreq(RCC_PERIPHCLK_SDMMC), which returns 0 because HAL_IS_BIT_SET(RCC->CR, RCC_CR_PLL1RDY) returns false (bit not set) at stm32h7xx_hal_rcc_ex.c line 2717 (firmware version V1.11.2). The HAL sees this zero return value and assumes something is wrong with the peripheral clock, and refuses to proceed with peripheral/card initialization.

This is of course incorrect, as I have SYSCLK fed from PLL1P and the system is stable, and SDMMC1 fed from PLL1Q and it also works with M7. With GDB I can read the RCC_CR register from both M7 and M4 perspective, and I see that on M7 it shows the PLLs as ready (RDY bits set), while on M4 those bits are clear.

What could be causing this? I read through some of the RCC section of the reference manual and it appears that the two cores have different access to RCC registers (but only sometimes...calling __HAL_RCC_SDMMC1_CLK_ENABLE() on M4 before it calls MX_SDMMC1_SD_Init() makes no difference).

I have tried fiddling with SDMMC1 clocks and modes to no avail. I also checked the errata sheet but there's no information about this in there. I assume that this is a software bug somewhere, probably in my configuration.

    This topic has been closed for replies.
    Best answer by SHs

    Hello @liamur ,

    Have you considered changing the clock source, such as using PLL2R? Additionally, have you explored our BootCM4_CM7 template in the reference firmware package? This project offers a comprehensive reference template that can be utilized to develop any firmware application involving both cores.

     

    Best Regards,

    1 reply

    SHsAnswer
    ST Employee
    August 30, 2024

    Hello @liamur ,

    Have you considered changing the clock source, such as using PLL2R? Additionally, have you explored our BootCM4_CM7 template in the reference firmware package? This project offers a comprehensive reference template that can be utilized to develop any firmware application involving both cores.

     

    Best Regards,

    liamurAuthor
    Visitor II
    September 2, 2024

    Thank you! Switching to PLL2R fixed the problem! M4 can now write to the SD card, albeit only at low speed and without MDMA. I may not even need DMA because the system is not transferring very much data.