STM32H7A3 flash CR register incorrectly defined in SVD and source
Specifically the SNB (SSN1 & SSN2 in the data sheet) bits are defined erroneously as being 3 bits wide at position 6, whereas it should be 7 bits wide, allowing all 128 sectors in each bank to be erased.
#define FLASH_CR_SNB_Pos (6U)
#define FLASH_CR_SNB_Msk (0x7FUL << FLASH_CR_SNB_Pos) /*!< 0x00001FC0 */
#define FLASH_CR_SNB FLASH_CR_SNB_Msk /*!< Sector erase selection number */
#define FLASH_CR_SNB_0 (0x01UL << FLASH_CR_SNB_Pos) /*!< 0x00000040 */
#define FLASH_CR_SNB_1 (0x02UL << FLASH_CR_SNB_Pos) /*!< 0x00000080 */
#define FLASH_CR_SNB_2 (0x04UL << FLASH_CR_SNB_Pos) /*!< 0x00000100 */
#define FLASH_CR_SNB_3 (0x08UL << FLASH_CR_SNB_Pos) /*!< 0x00000200 */
#define FLASH_CR_SNB_4 (0x10UL << FLASH_CR_SNB_Pos) /*!< 0x00000400 */
#define FLASH_CR_SNB_5 (0x20UL << FLASH_CR_SNB_Pos) /*!< 0x00000800 */
#define FLASH_CR_SNB_6 (0x40UL << FLASH_CR_SNB_Pos) /*!< 0x00001000 */This causes the HAL_FLASHEx_Erase to behave improperly.
The SVD is being used by the STM32-RS project and is causing incorrect code generation.