STM32H7B3 synchronous usart slave with a continuous clock
Hi!
I wonder if it is possible to set up the STM32H7B3 µC as a synchronous usart slave with the usart1 peripheral. From the reference manual it seems that it is only possible to set it up in 'SPI-mode'. The functionality I want is a USART slave that transmits data packets at a fixed rate(i.e. 1kHz) with no NSS, at the bit-rate determined by a continuous clock provided by the master.
Any clarification would be appreciated!