Skip to main content
Visitor II
May 31, 2021
Solved

STM32L072 UART bootLoader

  • May 31, 2021
  • 2 replies
  • 1157 views

I want to Implement the UART bootloader to the STM3272cz Microcontroller and flash the code with STM32cube programmer .I want to understand the STM32 cube programmer UART protocol used here for flashing the Bin file to the micro controller .

Any suggestions please help me in understanding the concept

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    AN2606 can be understood as the central point for all bootloader questions and also mentions the associated documents in section 2:

    • AN3154: CAN protocol used in the STM32 bootloader
    • AN3155: USART protocol used in the STM32 bootloader
    • AN3156: USB DFU protocol used in the STM32 bootloader
    • AN4221: I2C protocol used in the STM32 bootloader
    • AN4286: SPI protocol used in the STM32 bootloader
    • AN5405: FDCAN protocol used in the STM32 bootloader

    AN3155 is probably the appnote you are interested in.

    Good luck!

    If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

    /Peter

    2 replies

    Technical Moderator
    May 31, 2021

    AN2606 can be understood as the central point for all bootloader questions and also mentions the associated documents in section 2:

    • AN3154: CAN protocol used in the STM32 bootloader
    • AN3155: USART protocol used in the STM32 bootloader
    • AN3156: USB DFU protocol used in the STM32 bootloader
    • AN4221: I2C protocol used in the STM32 bootloader
    • AN4286: SPI protocol used in the STM32 bootloader
    • AN5405: FDCAN protocol used in the STM32 bootloader

    AN3155 is probably the appnote you are interested in.

    Good luck!

    If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

    /Peter

    Sshan.1Author
    Visitor II
    May 31, 2021

    Hi Peter ,

    Thanks for your reply and The AN3155 USART protocol is used same in the STM32cube Programmer also ??Please confirm