STM32L4 SDMMC Peripheral Problem
hello,
I use a custom board with an MCU STM32L462VETX and i try to create a file system over an SD CARD using the SDMMC peripheral .
the hardware connection between the sd card and the MCU are the same the eval board : STM32L476G-EVAL
I use a sandisk 16go sd card
I have used the STM32L4Cube V1.16 and CubeMX6.1.1
I used the YouTube video from ST : https://www.youtube.com/watch?v=I9KDN1o6924
The problem :
the f_open and f_mount with forced mount option return FR_DISK_ERR always
i checked also the community questions and topics like the problem of delay after power on in HAL driver.
So i search any idea or a support to resolve this problem because we must use the sd card to save data in our project.
#SDMMC #FatFS