STM32N657X0 SAI configuration / No clock output
Hey,
I tried to follow all the steps of this thread as good as possible. Still I have a faulty SAI Perpheral. The Problem is that the generatet FSYNC and BCK are too low. They are both also dependent on the PLL Frequency. For example if i set IC7 so that it has 12.288MHz the FSYNC is 2kHz (insted of 48kHz) and BCK is 512kHz (instead of 12.288 MHz).
When i set IC7 to 192MHz FSYNC is 31.3kHz and BCK is about 8MHz. Also if I set any other clock channel than IC7 to feed the SAI1 Peripheral, then there won't be any FSYNC or BCK anymore.
The D-Cache is working and doesn't give me an error as i followed this post: https://community.st.com/t5/stm32-mcus-embedded-software/stm32n6-using-dcache-with-freertos-and-sai-gpdma-usage/m-p/850823/highlight/true#M69398
I am running everything in Appli. Here are the settings:
SAI Setting:

GPDMA1 Setting: