STM32U0 using LPUART with Hardware Flow Control
Hi,
I would like to use LPUART3 to proceed the UART communication with hardware control flow enable.
However, I found that when the Send_UART_DATA there indeed has TX signal from LA, but CTS/RTS hasn't changed, only when system reset, those two pins just could get the status changed.

Here is the configuration of MX_LPUART3_UART_Init()
static void MX_LPUART3_UART_Init(void)
{
/* USER CODE BEGIN LPUART3_Init 0 */
// Enable LPUART3 clock
__HAL_RCC_LPUART3_CLK_ENABLE();
//Enable GPIOB clock
__HAL_RCC_GPIOB_CLK_ENABLE();
/* USER CODE END LPUART3_Init 0 */
/* USER CODE BEGIN LPUART3_Init 1 */
// Enable NVIC interrupt for LPUART3
HAL_NVIC_SetPriority(LPUART3_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(LPUART3_IRQn);
GPIO_InitTypeDef GPIO_InitStruct = {0};
/*Configure LPUART pins : UART communication */
// RTS/CTS pins
GPIO_InitStruct.Pin = GPIO_PIN_4 | GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF6_LPUART3;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
// TX/RX pins
GPIO_InitStruct.Pin = GPIO_PIN_6 | GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF6_LPUART3;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* USER CODE END LPUART3_Init 1 */
hlpuart3.Instance = LPUART3;
hlpuart3.Init.BaudRate = 57600;
hlpuart3.Init.WordLength = UART_WORDLENGTH_8B;
hlpuart3.Init.StopBits = UART_STOPBITS_1;
hlpuart3.Init.Parity = UART_PARITY_NONE;
hlpuart3.Init.Mode = UART_MODE_TX_RX;
hlpuart3.Init.HwFlowCtl = UART_HWCONTROL_RTS_CTS;
hlpuart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
hlpuart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
hlpuart3.FifoMode = UART_FIFOMODE_DISABLE;
if (HAL_UART_Init(&hlpuart3) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&hlpuart3, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&hlpuart3, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&hlpuart3) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN LPUART3_Init 2 */
/* USER CODE END LPUART3_Init 2 */
}And below is the code of sending UART data in main()
uint8_t cmd_a[]={0x11, 0x22, 0x33, 0x44, 0x55};
if (HAL_UART_Transmit_IT(&hlpuart3,cmd_a, sizeof(cmd_a)) != HAL_OK) {
printf("Failed to send command\r\n");
}And the related callback
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
{
/* Prevent unused argument(s) compilation warning */
//UNUSED(huart);
/* NOTE : This function should not be modified, when the callback is needed,
the HAL_UART_TxCpltCallback can be implemented in the user file. */
uart_transfer=false;
printf("Transfer completed callback\r\n");
if (HAL_UART_Receive_IT(&hlpuart3, rx_data, sizeof(rx_data)) != HAL_OK) {
printf("Failed to start reception\r\n");
} else {
printf("Started reception successfully\r\n");
}
}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
/* Prevent unused argument(s) compilation warning */
//UNUSED(huart);
/* NOTE : This function should not be modified, when the callback is needed,
the HAL_UART_RxCpltCallback can be implemented in the user file.
*/
if (huart->Instance == LPUART3)
{
printf("Rx Transfer completed callback\r\n");
// Print received bytes (assuming ASCII or printable format)
printf("Received data: ");
for (int i = 0; i < sizeof(rx_data); i++) {
printf("%02X ", rx_data[i]); // Print in hex format
}
printf("\r\n");
// Optionally, restart reception if expecting continuous data
if (HAL_UART_Receive_IT(&hlpuart3, rx_data, sizeof(rx_data)) != HAL_OK) {
printf("Failed to restart reception\r\n");
}
}
}
void HAL_UART_ErrorCallback(UART_HandleTypeDef *huart)
{
if (huart->Instance == LPUART3)
{
printf("UART error: 0x%08lx\r\n", huart->ErrorCode);
}
}Here is the IRQ setting
#define LPUART3_IRQn USART4_LPUART3_IRQn
#define LPUART3_IRQHandler USART4_LPUART3_IRQHandler
void USART4_LPUART3_IRQHandler(void)
{
/* USER CODE BEGIN USART4_LPUART3_IRQn 0 */
printf("LPUART3 IRQ triggered\r\n");
/* USER CODE END USART4_LPUART3_IRQn 0 */
HAL_UART_IRQHandler(&hlpuart3);
/* USER CODE BEGIN USART4_LPUART3_IRQn 1 */
/* USER CODE END USART4_LPUART3_IRQn 1 */
}
And below is the print out log whenever trying to send the TX data
-First try after reboot---------------
LPUART3 IRQ triggered
LPUART3 IRQ triggered
LPUART3 IRQ triggered
LPUART3 IRQ triggered
LPUART3 IRQ triggered
LPUART3 IRQ triggered
LPUART3 IRQ triggered
Transfer completed callback
Started reception successfully
-2nd try after 1st time---------------
LPUART3 IRQ triggered
LPUART3 IRQ triggered
LPUART3 IRQ triggered
LPUART3 IRQ triggered
LPUART3 IRQ triggered
LPUART3 IRQ triggered
LPUART3 IRQ triggered
Transfer completed callback
Failed to start reception
I would like to know whether the setting of configuration is unexpected? If yes, how should I fixed it?
Thanks,
CY