stm32u5 ux host hid with no vbus power
Hi,
I try to migrate the UX_Host_HID example on STM32U575I-EV to nucleo-u575zi-q.
STM32CubeIDE Version: 1.17.0
STM32CubeMX Version: 6.13.0
I duplicate all the settings relating to USB host options to mine.



In the middleware:




and then copy the source code from the Ux_Host_HID

After programming the firmware to my ev board, i plug the hid device to the CN15 USB connector. There is noting happened and no power react on my hid device.

Did i miss any settings to setup the USB host example??
how can i provide power to the hid device???
Any response will be appreciated.