Skip to main content
Visitor II
July 18, 2023
Question

STM32U575i-EV Ux_Host_MSC example hard fault

  • July 18, 2023
  • 2 replies
  • 1284 views

Hi All,

Cube MX version - 6.9.0

Software Package version - 1.3.0

I am using STM32U575i-EV evolution board and trying to run the Ux_Host_MSC example code.

I generated the code using STM32 Cube Mx using example selector option, I generated the code for IAR.

RRajb2_0-1689681219342.png

As per the below readme file.

/STM32Cube/Example/Ux_Host_MSC/readme.html

I have configured or connected below jumpers.

JP25 : UCPD_5V Jumper

JP6 (UCPD_SRC) : Please on this jumper UCPD_SNK02 is mentioned on board.

JP14 and JP15 : both are connected to 1-2.

after flashing the code I am hitting the hard fault, could you please let me know which are the settings I might need to do if I generate the code using cubemx. currently I have not done any modification through cubemx.

    This topic has been closed for replies.

    2 replies

    RRajb.2Author
    Visitor II
    July 21, 2023

    Could anyone from forum respond to this please?

    Technical Moderator
    July 27, 2023

    Hi @RRajb.2 ,

    Could you please try the example STM32CubeU5/Projects/STM32U575I-EV/Applications/USBX
    /Ux_Host_MSC as is in the STM32CubeU5 package without importing it with STM32CubeMX?

    Do you face the same issue?

    -Amel

    RRajb.2Author
    Visitor II
    August 7, 2023

    @Amel NASRI 

    I am still facing the same issue, not able to identify which function or peripheral causing the hard fault.