Skip to main content
Visitor II
May 4, 2022
Question

STM32U585 serial programming (Embedded Linux)

  • May 4, 2022
  • 2 replies
  • 1380 views

Hi,

Is there a way to program STM32U585 MCU via USART1 peripheral using Embedded Linux processor? Except BOOT0 pin and RESET pin of U5 MCU what else need to be done to get into Serial Programming mode? 

Thanks in advance,

Nenad

    This topic has been closed for replies.

    2 replies

    Super User
    May 4, 2022

    The correct RX and TX pins, see AN2606 Application note "STM32 microcontroller system memory boot mode". If you need more flexibility you might look into Open Bootloader https://github.com/STMicroelectronics/stm32-mw-openbl

    hth

    KnarfB

    Graduate II
    May 4, 2022

    The protocol is documented, assume it can be implemented on any platform you can code on.

    The STM32 doesn't care what Platform/OS you're using, it's agnostic.