STM32U5A5ZJ comparator interrupts
Hello,
We have a custom board based on the STM32U5A5ZJ, and are in the process of writing a zephyr driver for the two analog comparators on the MCU. Our use-case requires the driver to support interrupts on both comparators. Looking at the reference manual, it seems that the two comparator instances have dedicated interrupt lines going into the EXTI (lines 17 and 18). However, neither of these EXTI lines are mapped into the NVIC. Instead, the NVIC has a single IRQ line (no. 72) for COMP1/COMP2.
As a stop gap, we have enabled interrupts on COMP1, but are forced to use polling for detecting state changes on COMP2 (non-ideal). Hence, we were wondering how one could possibly use/enable both comparator interrupts simultaneously from a zephyr context?
Any tips/suggestions would be appreciated. Thanks!