Skip to main content
Graduate
August 8, 2024
Question

STM32U5G9 ADC weird DMA issue. Broken HAL driver?

  • August 8, 2024
  • 2 replies
  • 1796 views

I have a STM32U5G9 based board. I use 2 ADCs, ADC1 and ADC2 in independent mode.

I need to measure changing voltages with a lot digital noise filtering. I achieve this by setting ADC to sample the signal to a memory buffer via DMA, then averaging the noise, and if the average shows significant difference from the previous run - a notification is sent to the program to react.

The basic idea is simple - read data from ADC continuously, so - I used circular buffer.

After fixing the last HAL package issue with removed `HAL_PWREx_EnableVddA()` call (I added the call, it's necessary for the ADC to work), I managed to have my setup up and running.

However, the problem starts when I stop the conversion, and then want to start it up again. So:

 
`HAL_ADC_Start_DMA` call - passes with `HAL_OK`.
 
`HAL_ADC_Stop_DMA` call - passes with `HAL_OK`.
 
But then again `HAL_ADC_Start_DMA` call - fails with `HAL_ERROR`, and as I figured out, internally `ADC_Enable` function fails with a time out. That just tells me nothing. I read STM32 forum thread about very similar issue that turned out to be VddA missing. The problem I get is identical behavior, but the VddA is OK, and the problem is triggered not at the first ADC start, but after the ADC is restarted. BTW, I start, stop, then start again it manually. There is plenty of time between those operations.
 
What I already tried was completely deinitializing the ADC1 with `HAL_ADC_DeInit` after stopping and reinitializing it with `HAL_ADC_Init` before starting again. It didn't help. I tried to use `HAL_ADCEx_RegularStop_DMA` instead of `HAL_ADC_Stop_DMA`, I even tried to use both. Nothing helps. When I try to stop continuous conversion, the ADC cannot be enabled again, the only way to make it work ever again is to power-cycle the MCU or use the reset button.
 
That is a very serious problem to me, because my device's new version uses only one ADC with changing regular conversion group to measure 2 different voltages. The point is - I don't need to have it done simultaneously, I use one at a time, so I really need only one ADC with 2 inputs. However, I have different sampling rates, filtering and buffer sizes for the signals, so in order to switch my measurements I need to stop ADC, change regular conversion group setup, switch the buffer and start the ADC circular DMA again. However, currently I see I can only start my ADC only once in the application life time, it doesn't start after being stopped.
 
Please help me. I don't know what to do next with this issue.
    This topic has been closed for replies.

    2 replies

    Technical Moderator
    August 9, 2024

    Hello @HTD 

    According to the reference manual (RM0456) the software is allowed to set ADEN only when all bits of ADC_CR registers are 0 (ADCAL = 0, JADSTART = 0, ADSTART = 0, ADSTP = 0, ADDIS = 0 and ADEN = 0) except for bit ADVREGEN which must be 1 (and the software must have wait for the startup time of the voltage regulator)

    Saket_Om_0-1723192738795.png

    Please check if these conditions are ok on your setup before calling again HAL_ADC_Start_DMA.

    HTDAuthor
    Graduate
    August 9, 2024

    Ooopsie, I misread the register value. But it's not this:

    HTD_0-1723201264061.png

    As you see - the second pass (failed) passes through this check, so the CR state is valid.

    It breaks later:

    HTD_1-1723201398841.png

    Line 4347 - just ADC_FLAG_RDY is not getting set in time.

    Naturally, I checked what happens if I increase the timeout limit to 2 seconds, but obviously the ADC_FLAG_RDY doesn't get set at all, even one eternity later.

    Graduate II
    August 9, 2024

    So the HAL driver starts ADC calibration, but it doesn't wait for it to finish?

    HTDAuthor
    Graduate
    August 9, 2024

    @LCE wrote:

    So the HAL driver starts ADC calibration, but it doesn't wait for it to finish?


    My bad, I misread the bit position, it's not a calibration issue. Please check my edited reply, when I provide more details from the debugger.