Question
STM32U5G9J ADC HAL_ADC_Start results in an error.
HAL_ADC_Start on STM32U5G9J results in HAL error.
Initializing the ADC
/* ADC4 init function */
void MX_ADC4_Init(void)
{
/* USER CODE BEGIN ADC4_Init 0 */
/* USER CODE END ADC4_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC4_Init 1 */
/* USER CODE END ADC4_Init 1 */
/** Common config
*/
hadc4.Instance = ADC4;
hadc4.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV256;
hadc4.Init.Resolution = ADC_RESOLUTION_12B;
hadc4.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc4.Init.ScanConvMode = ADC4_SCAN_DISABLE;
hadc4.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc4.Init.LowPowerAutoPowerOff = ADC_LOW_POWER_NONE;
hadc4.Init.LowPowerAutoWait = DISABLE;
hadc4.Init.ContinuousConvMode = ENABLE;
hadc4.Init.NbrOfConversion = 2;
hadc4.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc4.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc4.Init.DMAContinuousRequests = DISABLE;
hadc4.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_LOW;
hadc4.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc4.Init.SamplingTimeCommon1 = ADC4_SAMPLETIME_1CYCLE_5;
hadc4.Init.SamplingTimeCommon2 = ADC4_SAMPLETIME_1CYCLE_5;
hadc4.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc4) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_8;
sConfig.Rank = ADC4_REGULAR_RANK_1;
sConfig.SamplingTime = ADC4_SAMPLINGTIME_COMMON_1;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_7;
sConfig.Rank = ADC4_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC4_Init 2 */
/* USER CODE END ADC4_Init 2 */
}
void HAL_ADC_MspInit(ADC_HandleTypeDef* adcHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
if(adcHandle->Instance==ADC4)
{
/* USER CODE BEGIN ADC4_MspInit 0 */
/* USER CODE END ADC4_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_ADCDAC;
PeriphClkInit.AdcDacClockSelection = RCC_ADCDACCLKSOURCE_HCLK;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/* ADC4 clock enable */
__HAL_RCC_ADC4_CLK_ENABLE();
__HAL_RCC_GPIOG_CLK_ENABLE();
/**ADC4 GPIO Configuration
PG0 ------> ADC4_IN7
PG1 ------> ADC4_IN8
*/
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);
/* ADC4 interrupt Init */
// HAL_NVIC_SetPriority(ADC4_IRQn, 0, 0);
// HAL_NVIC_EnableIRQ(ADC4_IRQn);
/* USER CODE BEGIN ADC4_MspInit 1 */
/* USER CODE END ADC4_MspInit 1 */
}
}
Reading:
if (HAL_ADC_Start(&hadc4) != HAL_OK)
{
printf("HAL_ADC_Start ERROR\n");
}
if (HAL_ADC_PollForConversion(&hadc4, 10) == HAL_OK)
{
uint16_t value = (uint16_t) HAL_ADC_GetValue(&hadc4);
printf("Value: %d\n", (uint32_t)value);
}
else
{
printf("HAL_ADC_PollForConversion ERROR\n");
}
What can be the problem?