Skip to main content
Graduate
April 28, 2024
Solved

STM32U5G9J-DK2 application example "Fx_NoR_Write_Read_File" is not working

  • April 28, 2024
  • 1 reply
  • 2009 views

I encountered an issue with the "Fx_NoR_Write_Read_File" application example. Upon running the application, it consistently triggers an error that redirects control flow to the Error_Handler() function within the app_filex.c file.

Note that STM32U5G9J-DK2 is a brand new board.

Application example location:

../STM32Cube/Repository/STM32Cube_FW_U5_V1.5.0/Projects/STM32U5G9J-DK2/Applications/FileX/Fx_NoR_Write_Read_File

Entering to app_filex.c function Error_Handler() here.

 nor_xspi_status = fx_media_format(&nor_xspi_flash_disk, // nor_xspi_flash_disk pointer
 fx_stm32_levelx_nor_driver, // Driver entry
 (VOID *)NOR_DEFAULT_DRIVER, // Device info pointer
 (UCHAR *) fx_nor_xspi_media_memory, // Media buffer pointer
 sizeof(fx_nor_xspi_media_memory), // Media buffer size
 FX_NOR_XSPI_VOLUME_NAME, // Volume Name
 FX_NOR_XSPI_NUMBER_OF_FATS, // Number of FATs
 32, // Directory Entries
 FX_NOR_XSPI_HIDDEN_SECTORS, // Hidden sectors
 LX_STM32_XSPI_FLASH_SIZE / FX_NOR_XSPI_SECTOR_SIZE, // Total sectors
 FX_NOR_XSPI_SECTOR_SIZE, // Sector size
 8, // Sectors per cluster
 1, // Heads
 1); // Sectors per track

 /* Check the format nor_xspi_status */
 if (nor_xspi_status != FX_SUCCESS)
 {
 Error_Handler();
 }

Could you please help me on this

    This topic has been closed for replies.
    Best answer by Mike_ST

    Hello,

    thank you for your report,

    I reproduced the problem and entered a ticket.

    Edit: Internal ticket number: 180260.

     

    1 reply

    Mike_STAnswer
    Technical Moderator
    April 29, 2024

    Hello,

    thank you for your report,

    I reproduced the problem and entered a ticket.

    Edit: Internal ticket number: 180260.

     

    digidhamuAuthor
    Graduate
    April 29, 2024

    Thanks @Mike_ST and will wait for your update.

    Visitor II
    June 11, 2024

    I also had the same issue, wish I saw this post a few days ago. I was trying to port the solution over to my custom project with unexplained errors. Then I ran the example application and also had this same issue. @Mike_ST do you know when an update will be coming?

    Thanks.