STM3G0B1 as I2C SLAVE with NoStretchMode. How to handle HAL_I2C_Slave_Seq_Transmit_IT?
I'm using STM3G0B1 as I2C SLAVE device with NVIC+NoStretchMode since I2C Master device doesn't support the clock stretching.
When HAL_I2C_AddrCallback is called (Read request from Master device), HAL_I2C_Slave_Seq_Transmit_IT seems not working because 0xFF is transmitted, not the expected value held by I2C_REGISTERS.
I guess 0xFF is the default value with NoStretchMode to respond immediately to the request.
How to resolve this issue? Is there a way to transmit the correct data with NoStretchMode for Read request?
hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_ENABLE;
...
void HAL_I2C_AddrCallback(I2C_HandleTypeDef *hi2c, uint8_t TransferDirection, uint16_t AddrMatchCode) {
if (TransferDirection == I2C_DIRECTION_TRANSMIT) {
if (HAL_I2C_Slave_Seq_Receive_IT(hi2c, ®Addr, 1, I2C_FIRST_FRAME) != HAL_OK) {
DBG_LOG("%s(%d): Error Receive Data", __func__, __LINE__);
return;
}
} else {
if (HAL_I2C_Slave_Seq_Transmit_IT(hi2c, I2C_REGISTERS + regAddr, 1, I2C_FIRST_FRAME) != HAL_OK) {
DBG_LOG("%s(%d): Error Transmit Data", __func__, __LINE__);
return;
}
}
}