STMCube32IDE 1.16.0 - Local file copy fails - files not present when importing example
With latest STM32CubeIDE:

when I try to import a project for U585 with ThreadX and NetX Duo, I get local file copy failure.
Issue #1 - you need to add more details/logs, so that we can know WHICH file / package is causing the issues. It's a guessing game now.
Issue #2 - the importer downloads some file, which has a license I should read. If you click there to read it - browser just says the file is not available!
Issue #3 - the README.md file is missing.

Is it because I can't read the license file? I did accept the terms and conditions (god knows what they were).
But, how do I know what other files are missing? Is the project now usable or not?
I have plenty of disk space available.
annek@jannek-P720:~$ df -h .
Filesystem Size Used Avail Use% Mounted on
/dev/nvme1n1p1 916G 305G 565G 36% /home
Connections to GitHub are otherwise working just fine.
- Multiple pushes & fetches done to GitHub today w/o issues.
jannek@jannek-P720:~$ ll STM32Cube/Repository/
total 360496
drwxrwxr-x 3 jannek jannek 4096 Aug 16 13:54 ./
drwxrwxr-x 3 jannek jannek 4096 Aug 16 13:50 ../
-rw-rw-r-- 1 jannek jannek 66113 Aug 16 13:50 en.prom-stm32h7rs-mcu-finder.jpg
drwxrwxr-x 8 jannek jannek 4096 Aug 16 13:54 STM32Cube_FW_U5_V1.6.0/
-rw-rw-r-- 1 jannek jannek 369059989 Aug 16 13:53 stm32cube_fw_u5_v160.zip