STR32F411RE Board for VL53L4CD (GUI)
Hello
I have a few questions
Situation Summary:
Development board: STM32F411RE
Sensor: VL53L4CD TOF sensor
Previous successful case: On the STM32F401RE board, setting the BOOT0 pin to 1 → uploading the BIN file via STM32CubeProgrammer → sensor operation verified successfully via GUI.
Current issue (STM32F411RE board):
Setting BOOT0 the same way as on the F401 → STM32CubeProgrammer connection is lost.
Using the adjacent JP1 pin (instead of the originally used one) → BIN file download succeeds.
Running the GUI program → board and COM port not detected.
Running "FLASH FW" in the GUI → port is detected, but the sensor shows a "not detected" message.
Note: Both the F401RE and F411RE boards use the JP1 pin next to the board’s power pins as the BOOT pin.
Question: What is the recommended method to make the sensor work properly with the GUI on the STM32F411RE board?
I would appreciate any guidance you could provide on this issue.
Please find my email address below.
thanks
email : whtndhks@it-m.co.kr