Struggle Using GPDMA Linkedlist on JPEG: GPDMA Input LL Stalls After One Node On STM32U5G9
Hello everyone,
I am working on the STM32U5G9ZJT6Q MCU and am trying to use the JPEG Encoder by feeding him data through a GPDMA linkedlist mode from RAM. The data to encode is an image of 640*480 8-bit grayscale image (the image is stored in a .c file ; for jpeg, i use tables 0, no chrominance in sight).
I am not using the HAL methods for jpeg/dma, eventhough the JPEG_DMA_StartProcess inside HAL_JPEG_Encode_DMA in stm32u5xx_hal_jpeg.h function seems to support dma linkedlist transfers.
I ran the JPEG_EncodingFromFLASH_DMA example for stm32u5g9 discovery kit, without issue, but having to work with normal dma transfers and having to handle the input/output in interrupts seems a bit off to me. I would like to use the linkedlist for simpler automation.
I configured the jpeg_rx (input) and jpeg_tx (output) dma transfers as linkedlists. The jpeg output works fine, the nodes are correctly updated and stream data as wanted.
However, the jpeg input dma stalls after the first node, eventhough the next node is correctly updated (not a LLR or SAR issue as it links to the right addresses).
Here is are the values for the number of dma transfers when the program stalls.

From my understanding, each jpeg_rx request allow to transfer 4 words (16 bytes) to the IFIFO (8-words long) half empty.
I set my transfer length to a multiple of 4 words (in my case GPDMA->BR1.BNDT = 9600) to avoid having a request leaving the IFIFO under the threshold, preventing any other request. Still, it doesn't work so there's definitely something I haven't understood (reason could be totally unrelated).
I tried changing the granularity of transfers completion, playing with the order of registers initialization as well as their values, enabling/disabling JPEG Header generation, I balanced the bandwidth on each ports (at least I tried all the port configuration without noticeable changes so I don't think the issue is from the different port allocations except for GPDMA.TR2.DREQ) as well as other configurations.
Why would the input DMA stall after the first node if it's not the case for the output? Do I need to manually rearm the GPDMA in interrupt for each transfer (thus having to use standard DMA)?
Note: The quantization tables are derived from the JPEG standard, the results with MX_JPEG_Init are the same as me for the basic config used for now so I didn't include the functions.
Here is my code draft (don't mind the missing functions/headers, I copy pasted the essential).
==== cfg.h ====
#include "stm32u5g9xx.h"
struct cfg_encoder_s {
JPEG_TypeDef *jpeg;
struct jpeg_dma_s {
DMA_Channel_TypeDef *gpdma;
uint32_t *nodes;
uint32_t mem_addr; // remove in the future
} in, out;
uint32_t length_encoded;
};
extern struct cfg_encoder_s enc;
void cfg_gpdma_jpeg_in(struct cfg_encoder_s *enc, uint32_t *src_buf);
void cfg_gpdma_jpeg_out(struct cfg_encoder_s *enc, uint32_t *dst_buf);
void cfg_gpdma_jpeg_in_nodes(struct cfg_encoder_s *enc);
void cfg_gpdma_jpeg_out_nodes(struct cfg_encoder_s *enc);
void cfg_jpeg(struct cfg_encoder_s *enc, uint8_t quality);
void jpeg_start(struct cfg_encoder_s *enc);
void jpeg_end(struct cfg_encoder_s *enc);
#define BURST_LENGTH 8
#define BURST_LENGTH_IN BURST_LENGTH
#define BURST_LENGTH_OUT BURST_LENGTH
#define RES_X 640 // has to be multiple of size MCU (8 or 16, 8 here)
#define RES_Y 480 // has to be multiple of size MCU (8 or 16, 8 here)
#define RES (RES_Y * RES_X)
#define SIZE_MCU_X 8
#define SIZE_MCU_Y 8
#define N_MCU_X (RES_X / SIZE_MCU_X)
#define N_MCU_Y (RES_Y / SIZE_MCU_Y)
#define N_MCU_TOTAL (N_MCU_X * N_MCU_Y)
#define L_BUF_IN (RES / 1)
#define N_SUB_BUF_IN 8
#define L_SUB_BUF_IN (L_BUF_IN / N_SUB_BUF_IN)
#define L_NODE_IN L_SUB_BUF_IN
#define N_NODE_IN N_SUB_BUF_IN
#define L_BUF_OUT (RES / 1)
#define N_SUB_BUF_OUT 8
#define L_SUB_BUF_OUT (L_BUF_OUT / N_SUB_BUF_OUT)
#define L_NODE_OUT L_SUB_BUF_OUT / 4
#define N_NODE_OUT N_SUB_BUF_OUT==== cfg.c ====
#include "cfg.h"
struct cfg_encoder_s enc = {0};
static uint32_t cfg_nodes_in[N_NODE_IN][8] __attribute__((aligned(4))) = {0};
static uint32_t cfg_nodes_out[N_NODE_OUT][8] __attribute__((aligned(4))) = {0};
void cfg_gpdma_jpeg_in(struct cfg_encoder_s *enc, uint32_t *src_buf) {
uint32_t ccr, dar, sar, tr1, tr2, llr, la;
const uint32_t br1 = L_NODE_IN & 0xffff; // fixed
enc->in.gpdma->CCR &= ~(1 << DMA_CCR_EN_Pos); // disable dma during config
enc->in.gpdma->CCR |= (1 << DMA_CCR_RESET_Pos); // reset gpdma channel
ccr = enc->in.gpdma->CCR & ~(0xc37f07); // reserved bit mask
ccr |= (0b10 << DMA_CCR_PRIO_Pos); /* prio */
ccr |= (1 << DMA_CCR_LAP_Pos); /* linkedlist allocated port */
ccr |= (0 << DMA_CCR_LSM_Pos); /* link step mode */ // channel completed at last LLI (0) or ONCE for the current LLI (1)
ccr |= (0 << DMA_CCR_TOIE_Pos); /* trigger ovr ITE */
ccr |= (0 << DMA_CCR_SUSPIE_Pos); /* cplt susp ITE */
ccr |= (1 << DMA_CCR_USEIE_Pos); /* user setting error ITE */
ccr |= (1 << DMA_CCR_ULEIE_Pos); /* update link trsfer error ITE */
ccr |= (1 << DMA_CCR_DTEIE_Pos); /* data trfr error ITE */
ccr |= (0 << DMA_CCR_HTIE_Pos); /* HT cplt ITE */
ccr |= (1 << DMA_CCR_TCIE_Pos); /* T cplt ITE */
ccr |= (0 << DMA_CCR_SUSP_Pos); /* susp */
ccr |= (0 << DMA_CCR_RESET_Pos); /* reset */
enc->in.gpdma->CCR = ccr;
tr1 = enc->in.gpdma->CTR1 & ~(0xcffbfbfb); // reserved bit mask
tr1 |= (0 << DMA_CTR1_DSEC_Pos); /* dest sec */
tr1 |= (0 << DMA_CTR1_DAP_Pos); /* dest port */
tr1 |= (0 << DMA_CTR1_DHX_Pos); /* dest half word exch */
tr1 |= (0 << DMA_CTR1_DBX_Pos); /* dest byte exch */
tr1 |= ((BURST_LENGTH_IN-1) << DMA_CTR1_DBL_1_Pos); /* dest burst size of length (value-1) */
tr1 |= (0 << DMA_CTR1_DINC_Pos); /* dest inc */
tr1 |= (0b10 << DMA_CTR1_DDW_LOG2_Pos); /* dst data width of burst */
tr1 |= (0 << DMA_CTR1_SSEC_Pos); /* src sec */
tr1 |= (1 << DMA_CTR1_SAP_Pos); /* src port */
tr1 |= (0 << DMA_CTR1_SBX_Pos); /* src byte exch */
tr1 |= (0 << DMA_CTR1_PAM_Pos); /* align/padding */
tr1 |= ((BURST_LENGTH_IN-1) << DMA_CTR1_SBL_1_Pos); /* src burst size of length */
tr1 |= (1 << DMA_CTR1_SINC_Pos); /* src inc */
tr1 |= (0b10 << DMA_CTR1_SDW_LOG2_Pos); /* src data width burst */
tr2 = enc->in.gpdma->CTR2 & ~(0xc37fce7f); // reserved bit mask
tr2 |= (0b00 << DMA_CTR2_TCEM_Pos); /* trigger cplt transfer event mode */
tr2 |= (0b00 << DMA_CTR2_TRIGPOL_Pos); /* trigger event polarity */
tr2 |= (0 << DMA_CTR2_TRIGSEL_Pos); /* trigger event selection (no) */
tr2 |= (0 << DMA_CTR2_TRIGM_Pos); /* trigger mode */
tr2 |= (1 << DMA_CTR2_BREQ_Pos); /* block hw req (burst level ?) */
tr2 |= (1 << DMA_CTR2_DREQ_Pos); /* dest hw req (by a periph?) */ // 1: dest req hw, 0: src """"
tr2 |= (0 << DMA_CTR2_SWREQ_Pos); /* software req */
tr2 |= (124 << DMA_CTR2_REQSEL_Pos); /* gpdma hw req selection (jpeg_rx) */
dar = (uint32_t) &enc->jpeg->DIR; // fixed
enc->in.mem_addr = (uint32_t) &src_buf[0];
sar = enc->in.mem_addr; // to be updated
// Link first node to register for init
enc->in.nodes = &cfg_nodes_in[0][0];
la = ((uint32_t) enc->in.nodes) & 0xfffc;
llr = la | (1 << DMA_CLLR_ULL_Pos) | (0b11111 << DMA_CLLR_UDA_Pos); // (UT1-UT2-UB1-USA-UDA) update fields, LBA->LLR
enc->in.gpdma->CLLR = llr;
enc->in.gpdma->CLBAR = ((uint32_t) enc->in.nodes) & 0xffff0000;
// Link 2d node to the first one for update
la = ((uint32_t) &cfg_nodes_in[1][0]) & 0xfffc;
llr = la | (1 << DMA_CLLR_ULL_Pos) | (0b00010 << DMA_CLLR_UDA_Pos);
// init first node with full parameters
// tr1, tr2, br1, sar, dar, llr
cfg_nodes_in[0][0] = tr1;
cfg_nodes_in[0][1] = tr2;
cfg_nodes_in[0][2] = br1;
cfg_nodes_in[0][3] = sar;
cfg_nodes_in[0][4] = dar;
cfg_nodes_in[0][5] = llr;
return;
}
void cfg_gpdma_jpeg_out(struct cfg_encoder_s *enc, uint32_t *dst_buf) {
uint32_t ccr, dar, sar, tr1, tr2, llr, la;
const uint32_t br1 = L_NODE_OUT & 0xffff; // fixed
enc->out.gpdma->CCR &= ~(1 << DMA_CCR_EN_Pos); // disable dma during config
enc->out.gpdma->CCR |= (1 << DMA_CCR_RESET_Pos); // reset gpdma channel
ccr = enc->out.gpdma->CCR & ~(0xc37f07);
ccr |= (0b10 << DMA_CCR_PRIO_Pos); /* prio */
ccr |= (1 << DMA_CCR_LAP_Pos); /* linkedlist allocated port */
ccr |= (0 << DMA_CCR_LSM_Pos); /* link step mode */ // channel completed at last LLI (0) or ONCE for the current LLI (1)
ccr |= (0 << DMA_CCR_TOIE_Pos); /* trigger ovr ITE */
ccr |= (0 << DMA_CCR_SUSPIE_Pos); /* cplt susp ITE */
ccr |= (1 << DMA_CCR_USEIE_Pos); /* user setting error ITE */
ccr |= (1 << DMA_CCR_ULEIE_Pos); /* update link trsfer error ITE */
ccr |= (1 << DMA_CCR_DTEIE_Pos); /* data trfr error ITE */
ccr |= (0 << DMA_CCR_HTIE_Pos); /* HT cplt ITE */
ccr |= (1 << DMA_CCR_TCIE_Pos); /* T cplt ITE */
ccr |= (0 << DMA_CCR_SUSP_Pos); /* susp */
ccr |= (0 << DMA_CCR_RESET_Pos); /* reset */
enc->out.gpdma->CCR = ccr;
tr1 = enc->out.gpdma->CTR1 & ~(0xcffbfbfb);
tr1 |= (0 << DMA_CTR1_DSEC_Pos); /* dest sec */
tr1 |= (1 << DMA_CTR1_DAP_Pos); /* dest port */
tr1 |= (0 << DMA_CTR1_DHX_Pos); /* dest half word exch ??*/
tr1 |= (0 << DMA_CTR1_DBX_Pos); /* dest byte exch ??*/
tr1 |= ((BURST_LENGTH_OUT-1) << DMA_CTR1_DBL_1_Pos); /* dest burst size of length (value-1) */
tr1 |= (1 << DMA_CTR1_DINC_Pos); /* dest inc */
tr1 |= (0b10 << DMA_CTR1_DDW_LOG2_Pos); /* dst data width of burst */
tr1 |= (0 << DMA_CTR1_SSEC_Pos); /* src sec */
tr1 |= (0 << DMA_CTR1_SAP_Pos); /* src port */
tr1 |= (0 << DMA_CTR1_SBX_Pos); /* src byte exch ?? */
tr1 |= (0 << DMA_CTR1_PAM_Pos); /* align/padding (osef if burst_size = data_size */
tr1 |= ((BURST_LENGTH_OUT-1) << DMA_CTR1_SBL_1_Pos); /* src burst size of length */
tr1 |= (0 << DMA_CTR1_SINC_Pos); /* src inc */
tr1 |= (0b10 << DMA_CTR1_SDW_LOG2_Pos); /* src data width burst */
tr2 = enc->out.gpdma->CTR2 & ~(0xc37fce7f);
tr2 = (0b00 << DMA_CTR2_TCEM_Pos); /* trigger cplt transfer event mode */
tr2 |= (0b00 << DMA_CTR2_TRIGPOL_Pos); /* trigger event polarity */
tr2 |= (0 << DMA_CTR2_TRIGSEL_Pos); /* trigger event selection (no) */
tr2 |= (0 << DMA_CTR2_TRIGM_Pos); /* trigger mode */
tr2 |= (1 << DMA_CTR2_BREQ_Pos); /* block hw req (burst level ?) */
tr2 |= (0 << DMA_CTR2_DREQ_Pos); /* dest hw req (by a periph?) */ // 1: dest req hw, 0: src """"
tr2 |= (0 << DMA_CTR2_SWREQ_Pos); /* software req */
tr2 |= (125 << DMA_CTR2_REQSEL_Pos); /* gpdma hw req selection (jpeg_tx) */
sar = (uint32_t) &enc->jpeg->DOR; // fixed
enc->out.mem_addr = (uint32_t) &dst_buf[0];
dar = enc->out.mem_addr; // to be updated
enc->out.nodes = &cfg_nodes_out[0][0];
la = ((uint32_t) enc->out.nodes) & 0xfffc;
llr = la | (1 << DMA_CLLR_ULL_Pos) | (0b11111 << DMA_CLLR_UDA_Pos); // (UT1-UT2-UB1-USA-UDA) update fields, LBA->LLR
// Link first node to register for init
enc->out.gpdma->CLLR = llr;
enc->out.gpdma->CLBAR = ((uint32_t) enc->out.nodes) & 0xffff0000;
// Link 2d node to the first one for update
la = ((uint32_t) &cfg_nodes_out[1][0]) & 0xfffc;
llr = la | (1 << DMA_CLLR_ULL_Pos) | (0b00001 << DMA_CLLR_UDA_Pos);
// init first node with full parameters
// tr1, tr2, br1, sar, dar, llr
cfg_nodes_out[0][0] = tr1;
cfg_nodes_out[0][1] = tr2;
cfg_nodes_out[0][2] = br1;
cfg_nodes_out[0][3] = sar;
cfg_nodes_out[0][4] = dar;
cfg_nodes_out[0][5] = llr;
return;
}
void cfg_jpeg(struct cfg_encoder_s *enc, uint8_t quality) {
enc->length_encoded = 0;
uint32_t tmp;
tmp = enc->jpeg->CR & ~(0x787f);
tmp |= (1 << JPEG_CR_OFF_Pos); /* flush output fifo */
tmp |= (1 << JPEG_CR_IFF_Pos); /* flush input fifo */
tmp |= (0 << JPEG_CR_ODMAEN_Pos); /* en out dma */ // disable dma for cfg
tmp |= (0 << JPEG_CR_IDMAEN_Pos); /* en in dma */
tmp |= (0 << JPEG_CR_HPDIE_Pos); /* en header parsing done interrupt */
tmp |= (1 << JPEG_CR_EOCIE_Pos); /* en end of conversion interrupt */
tmp |= (0 << JPEG_CR_OFNEIE_Pos); /* en output fifo not empty interrupt */
tmp |= (0 << JPEG_CR_OFTIE_Pos); /* en output fifo threshold interrupt */
tmp |= (0 << JPEG_CR_IFNFIE_Pos); /* en input fifo not empty interrupt */
tmp |= (0 << JPEG_CR_IFTIE_Pos); /* en input fifo not full interrupt */
tmp |= (1 << JPEG_CR_JCEN_Pos); /* en jpeg core */
enc->jpeg->CR = tmp;
enc->jpeg->CONFR0 &= ~(1 << JPEG_CONFR0_START_Pos);
tmp = enc->jpeg->CONFR1 & ~(0xffff01fb);
tmp |= (RES_Y << JPEG_CONFR1_YSIZE_Pos); /* YSIZE nb lines in src img */
tmp |= (0 << JPEG_CONFR1_HDR_Pos); /* enable header gen/parsing */
tmp |= (0b00 << JPEG_CONFR1_NS_Pos); /* reg = [nb compo. - 1] for scan hdr */
tmp |= (0b00 << JPEG_CONFR1_COLORSPACE_Pos); /* color space */ // 00 for grayscale, 01 for YUV
tmp |= (0 << JPEG_CONFR1_DE_Pos); /* 0 encode mode, 1 decode */
tmp |= (0 << JPEG_CONFR1_NF_Pos); /* reg = [nb of color components - 1] */
enc->jpeg->CONFR1 = tmp;
// max 67108863 (1<<26)-1
tmp = enc->jpeg->CONFR2 & ~(0x3ffffff);
tmp |= ((N_MCU_TOTAL - 1) << JPEG_CONFR2_NMCU_Pos); // reg[0:25] = [nb mcu to encode - 1]
enc->jpeg->CONFR2 = tmp;
tmp = enc->jpeg->CONFR3 & ~(0xffff << 16);
tmp |= (RES_X << JPEG_CONFR3_XSIZE_Pos); // nb pixel per line (16 bit value)
enc->jpeg->CONFR3 = tmp;
// Y8 1 block of 8x8 data
tmp = enc->jpeg->CONFR4 & ~0xffff;
tmp |= (1 << JPEG_CONFR4_HSF_Pos); /* hori sampling factor */ // 1 -> no subsampling
tmp |= (1 << JPEG_CONFR4_VSF_Pos); /* vert sampling factor */
tmp |= (0 << JPEG_CONFR4_NB_Pos); /* nb of blocks to a particular color in the MCU (Y-1) */
tmp |= (0b00 << JPEG_CONFR4_QT_Pos); /* Quant table used */
tmp |= (0 << JPEG_CONFR4_HA_Pos); /* select ac huff table (0 or 1) */
tmp |= (0 << JPEG_CONFR4_HD_Pos); /* select dc huff table (0 or 1) */
enc->jpeg->CONFR4 = tmp;
// unused CONFRx, reset them
enc->jpeg->CONFR5 &= ~0xffff;
enc->jpeg->CONFR6 &= ~0xffff;
enc->jpeg->CONFR7 &= ~0xffff;
set_tables(enc, quality); // from ITU CCITT T.81 JPEG ISO/IEC 10918-1 guidelines
return;
}
static void init_node(uint32_t nodes[8], uint32_t config[8], uint8_t curr_idx, uint8_t n) {
for(int i = 0; i < n; i++)
nodes[i] = config[i];
return;
}
// destination buffer is fixed, jpeg->dir
void cfg_gpdma_jpeg_in_nodes(struct cfg_encoder_s *enc) {
const uint32_t br1 = cfg_nodes_in[0][2];
uint32_t sar;
uint32_t llr;
uint32_t la;
uint32_t top_idx;
for(top_idx = 1; top_idx < N_NODE_IN - 1; top_idx++) {
sar = enc->in.mem_addr + (((top_idx) * br1) % L_BUF_IN);
la = ((uint32_t) &cfg_nodes_in[top_idx+1][0]) & 0xfffc;
llr = la | (0b00010 << DMA_CLLR_UDA_Pos) | (1 << DMA_CLLR_ULL_Pos); // (UT1-UT2-UB1-USA-UDA) update fields order
init_node(cfg_nodes_in[top_idx], (uint32_t [8]) {sar, llr}, top_idx, 2); // only sar and llr updated
}
// last node + circular mode
sar = (uint32_t) enc->in.mem_addr;
la = ((uint32_t) &cfg_nodes_in[1][0]) & 0xfffc;
llr = la | (0b11111 << DMA_CLLR_UDA_Pos) | (1 << DMA_CLLR_ULL_Pos);
init_node(cfg_nodes_in[top_idx], (uint32_t [8]){sar, llr}, top_idx, 2);
return;
}
void cfg_gpdma_jpeg_out_nodes(struct cfg_encoder_s *enc) {
const uint32_t br1 = L_NODE_OUT & 0xffff;
uint32_t dar;
uint32_t llr;
uint32_t la;
uint8_t top_idx;
for(top_idx = 1; top_idx < N_NODE_OUT - 1; top_idx++) {
dar = (uint32_t) enc->out.mem_addr + (((top_idx) * br1) % L_BUF_OUT);
la = ((uint32_t) &cfg_nodes_out[top_idx+1][0]) & 0xfffc;
llr = la | (0b00001 << DMA_CLLR_UDA_Pos) | (1 << DMA_CLLR_ULL_Pos); // (UT1-UT2-UB1-USA-UDA) update fields
init_node(cfg_nodes_out[top_idx], (uint32_t [8]) {dar, llr}, top_idx, 2); // only dar and llr updated
}
// last node + circular mode
dar = (uint32_t) enc->out.mem_addr;
la = ((uint32_t) &cfg_nodes_out[1][0]) & 0xfffc;
llr = la | (0b11111 << DMA_CLLR_UDA_Pos) | (1 << DMA_CLLR_ULL_Pos);
init_node(cfg_nodes_out[top_idx], (uint32_t [8]){dar, llr}, top_idx, 2);
return;
}
void jpeg_start(struct cfg_encoder_s *enc) {
// move flush I/OFIFO from cfg here
enc->jpeg->CONFR0 |= (1 << JPEG_CONFR0_START_Pos);
enc->out.gpdma->CCR |= (1 << DMA_CCR_EN_Pos);
enc->in.gpdma->CCR |= (1 << DMA_CCR_EN_Pos);
enc->jpeg->CR |= (1 << JPEG_CR_ODMAEN_Pos) | (1 << JPEG_CR_IDMAEN_Pos);
return;
}
//supposed to be put in EOC as a callback function
void jpeg_end(struct cfg_encoder_s *enc) {
if(!(enc->jpeg->SR & (1 << JPEG_SR_OFNEF_Pos)))
return;
// suspend transfer when fifo dma empty, wait for it to be suspended, then manually extract data from fifo gpdma
while((enc->out.gpdma->CSR & (0b11111111 << DMA_CSR_FIFOL_Pos)) != 0); // wait until there is no data left in fifo
enc->out.gpdma->CCR |= (1 << DMA_CCR_SUSP_Pos); // suspend
while(enc->out.gpdma->CSR & (1 << DMA_CSR_SUSPF_Pos)); // wait until suspend
enc->length_encoded += L_NODE_OUT - (enc->out.gpdma->CBR1 & 0xffff); // sub to the remaining item transfers in BNDT
while((enc->jpeg->SR & (1 << JPEG_SR_OFNEF_Pos)) != 0) { // 4 bytes=1 word
*(uint32_t *) (enc->out.mem_addr + enc->length_encoded % L_BUF_OUT) = enc->jpeg->DOR;
enc->length_encoded += 4;
}
enc->jpeg->CR |= (1 << JPEG_CR_OFF_Pos) | (1 << JPEG_CR_IFF_Pos);
enc->in.gpdma->CCR |= (1 << DMA_CCR_RESET_Pos);
enc->out.gpdma->CCR |= (1 << DMA_CCR_RESET_Pos);
}==== main.h ====
#include "img.h"
#include "cfg.h"
#include "stm32u5xx_hal.h"
#define JPEG_IN_DMA_IRQn ((IRQn_Type) GPDMA1_Channel0_IRQn)
#define JPEG_IN_DMA_CH ((DMA_Channel_TypeDef *) GPDMA1_Channel0_BASE_NS)
#define JPEG_OUT_DMA_IRQn ((IRQn_Type) GPDMA1_Channel1_IRQn)
#define JPEG_OUT_DMA_CH ((DMA_Channel_TypeDef *) GPDMA1_Channel1_BASE_NS)
void Error_Handler(void);
void dma_in_cplt(DMA_HandleTypeDef *hdma);
void dma_out_cplt(DMA_HandleTypeDef *hdma);
extern uint32_t jpeg_cplt;
extern uint32_t dma_in_error;
extern uint32_t dma_out_error;
extern struct cfg_encoder_s *jpeg_enc;==== main.c ====
extern uint8_t img[IMG_RES] __attribute__((aligned(4))) ;
extern uint8_t img_jpeg[IMG_RES] __attribute__((aligned(4))) ;
int main(void)
{
HAL_Init();
SystemPower_Config();
SystemClock_Config();
__HAL_RCC_GPDMA1_CLK_ENABLE();
__HAL_RCC_JPEG_CLK_ENABLE();
HAL_NVIC_SetPriority(JPEG_IN_DMA_IRQn, 6, 0);
HAL_NVIC_SetPriority(JPEG_OUT_DMA_IRQn, 7, 0);
HAL_NVIC_SetPriority(JPEG_IRQn, 8, 0);
HAL_NVIC_EnableIRQ(JPEG_IN_DMA_IRQn);
HAL_NVIC_EnableIRQ(JPEG_OUT_DMA_IRQn);
HAL_NVIC_EnableIRQ(JPEG_IRQn);
MX_ICACHE_Init();
jpeg_enc->in.gpdma = (DMA_Channel_TypeDef*) JPEG_IN_DMA_CH;
jpeg_enc->out.gpdma = (DMA_Channel_TypeDef*) JPEG_OUT_DMA_CH;
jpeg_enc->jpeg = (JPEG_TypeDef*) JPEG;
cfg_jpeg(jpeg_enc, 75);
cfg_gpdma_jpeg_in(jpeg_enc, (uint32_t*) img);
cfg_gpdma_jpeg_in_nodes(jpeg_enc);
cfg_gpdma_jpeg_out(jpeg_enc, (uint32_t*) img_jpeg);
cfg_gpdma_jpeg_out_nodes(jpeg_enc);
jpeg_start(jpeg_enc);
while (!jpeg_cplt && !dma_out_error && !dma_in_error) {}
}
void dma_in_cplt(DMA_HandleTypeDef *hdma) {
dma_in_cnt++;
}
void dma_out_cplt(DMA_HandleTypeDef *hdma) {
dma_out_cnt++;
jpeg_enc->length_encoded += L_NODE_OUT;
}==== stm32u5xx_it.c ====
extern uint32_t jpeg_cplt;
extern uint32_t dma_in_error;
extern uint32_t dma_out_error;
extern struct cfg_encoder_s *jpeg_enc;
union dma_sr_u { // just to see regs without using SFRs
uint32_t data;
struct {
uint32_t idlef:1;
uint32_t reserved_0:7;
uint32_t tcf:1;
uint32_t htf:1;
uint32_t dtef:1;
uint32_t ulef:1;
uint32_t usef:1;
uint32_t suspf:1;
uint32_t tof:1;
uint32_t reserved_1:1;
uint32_t fifol:8;
uint32_t reserved_2:8;
};
};
void GPDMA1_Channel0_IRQHandler(void)
{
jpeg_in_dma_irq();
return;
}
void GPDMA1_Channel1_IRQHandler(void)
{
jpeg_out_dma_irq();
return;
}
static void jpeg_in_dma_irq() {
DMA_Channel_TypeDef *dma = (DMA_Channel_TypeDef*)JPEG_IN_DMA_CH;
union dma_sr_u sr = {.data=dma->CSR};
if(sr.tcf) {
dma->CFCR |= (1 << DMA_CFCR_TCF_Pos);
dma_in_cplt(&handle_GPDMA1_Channel1);
}
if(sr.htf)
dma->CFCR |= (1 << DMA_CFCR_HTF_Pos);
if(sr.usef)
dma->CFCR |= (1 << DMA_CFCR_USEF_Pos);
if(sr.ulef)
dma->CFCR |= (1 << DMA_CFCR_ULEF_Pos);
if(sr.dtef)
dma->CFCR |= (1 << DMA_CFCR_DTEF_Pos);
if(sr.tof)
dma->CFCR |= (1 << DMA_CFCR_TOF_Pos);
return;
}
static void jpeg_out_dma_irq() {
DMA_Channel_TypeDef *dma = (DMA_Channel_TypeDef*)JPEG_OUT_DMA_CH;
union dma_sr_u sr = {.data=dma->CSR};
if(sr.tcf) {
dma->CFCR |= (1 << DMA_CFCR_TCF_Pos);
dma_out_cplt(&handle_GPDMA1_Channel0);
}
if(sr.htf)
dma->CFCR |= (1 << DMA_CFCR_HTF_Pos);
if(sr.usef)
dma->CFCR |= (1 << DMA_CFCR_USEF_Pos);
if(sr.ulef)
dma->CFCR |= (1 << DMA_CFCR_ULEF_Pos);
if(sr.dtef)
dma->CFCR |= (1 << DMA_CFCR_DTEF_Pos);
if(sr.tof)
dma->CFCR |= (1 << DMA_CFCR_TOF_Pos);
return;
}