Synopsis OTG_FS controller - how raw data are processed ?
Dear Community,
I was trying to make composite USB2.0 device (FullSpeed) consisting of a UVC and HID component. Both the components I’ve tested before as a standalone device successfully. However after making a composite device accordingly to the HID-CDC example in the STM32F105/7xx, STM32F2xx and STM32F4xx USB On-The-Go Host and Device Library I found myself lost. Using a hardware USB analyzer (and some help from OSR community) I found so far that after receiving the composite device descriptor by the PC host a class request (0x0A) failed with the USB analyzer message: �?The device was not able to process this request. At least one transaction contains a STALL token, which means that the device did not expect this request. “
The payload of the failing class request is:
0x21 0x0A 0x00 0x00 0x02 0x00 0x00 0x00
Accordingly to usb in a nutshell (https://www.beyondlogic.org/usbnutshell/usb6.shtml) this means it is a class request for the device having the bRequest value: 0x0A.(USB_REQ_GET_INTERFACE) which should either be dispatched into the video class driver or hid class driver.
Since it is to me not clear how the Synopsis FS_OTG core inside the Stm32F407 is processing the raw data from the bus I would be very glad if someone could post a link with information regarding this.