Skip to main content
Graduate
February 14, 2025
Question

SysTick not incrementing with TrustZone enabled

  • February 14, 2025
  • 1 reply
  • 671 views

I have a simple project set up for the stm32h573II-DK that has USART1 set up and I can print to serial out over the same USB connector that uses ST-LINK with HAL_UART_Transmit(&hcom_uart[COM1], MSG, sizeof(MSG), 100);. I can not use HAL_Delay(1000); to print every ~1 second. When entering the HAL_Delay function, I can see with a debugger that uwTick is never incremented and with breakpoints I can see that the systick handler is never called. I made a project that doesn't have TrustZone set up and it can print every one second. I do not think this is an ISR priority issue, as I am calling HAL_Delay() from main(). All of the code was generated with cubemx and the only edits I've made were to add the print. What could I be doing wrong to prevent the systick interrupt from being handled correctly?

    This topic has been closed for replies.

    1 reply

    ST Employee
    April 3, 2025

    Hello @chipchop

    The SysTick timer is used as the timebase in the default HAL implementation, is this issue within an RTOS context?