Skip to main content
Visitor II
September 22, 2021
Question

The example with FileX on STM32H735G-DK is not working with exFAT SD cards.

  • September 22, 2021
  • 1 reply
  • 695 views

I tried using the example Fx_uSD_File_Edit for the discovery kit: STM32H735G which works fine.

But when changing the configuration in .ioc file to exFAT instead of FAT and using an SD card formated in standard exFAT the example goes into an error. The error comes in the following function: SDMMC_GetCmdResp1(). The first do while loop is returning an SDMMC_ERROR_TIMEOUT.

The problem is that I need exFAT to store a big amount of data (>32GB) and FAT don't fit.

Thank you very much for your help.

    This topic has been closed for replies.

    1 reply

    Visitor II
    September 22, 2021

    Hello @Freistyle​ ,

    Your issue has been internally raised. I will keep you informed.

    Thanks for you contribution.

    BeST Regards,

    Walid