Skip to main content
Visitor II
February 1, 2023
Question

The STM32F469 has the USB bugs found in errata of STM32F429 (but not its own errata) where it can't connect to low-speed thru a hub. Is that a problem in the PHY, and will using an external PHY solve it?

  • February 1, 2023
  • 1 reply
  • 660 views

Specifically, will using the STULPI01 allow a low-speed device to connect via a hub to the OTG-HS USB interface, or is this bug not actually in the internal FS-PHY, but in the controller?

    This topic has been closed for replies.