The USB MSC Host library of FW_F7_V_17.1 in STM32F746-DISCOVERY does not work completely. Can you help me?
I was working with an example of the FW_F7_V_16.1 version and it works perfectly. When upgrading to version 17.1 I get an error "Error: Cannot Open USBHost.txt".
Checking a bit I found that the difference is mainly in the files:
usb_ctlreq.h and usbclreq.c
I suspect the ParseCfgDesc & ParseEPDesc functions.
However there are details I don't understand and I couldn't find out more.
Searching in the community I found the link to update the version and coincidentally the above mentioned files, where an update is mentioned
We confirm the issue that is in USB Host library V3.4.1 and that was fixed in V3.5.0.
STM32F7 CubeFW release still doesn't integrate USB Host V3.5.0, but you can get it here on GitHub and use it in your package to fix the problem.
Future updates of STM32F7 package will contain V3.5.1.
However I downloaded it and updated it in my project and the problem was corrected "I can now write the file".
The problem now is that when viewing the USB drive directory I see files that were never created.