Threadx thread gets suspended from EMC interference
Im using USBx as my USB driver for the STM32U599VJT6Q.
This driver has 2 functions: "usbx_cdc_acm_read_thread_entry" and "usbx_cdc_acm_write_thread_entry" each of which runs in their own thread.
The problem im having is the thread running "usbx_cdc_acm_write_thread_entry" gets semaphore suspended whenever interference occurs on the USB transmission line.
The problem appears to be related to the function "ux_device_class_cdc_acm_write" as i have not been able to recreate the issue after removing it from the function.
I haven't found any functions that can circumvent a semaphore suspension, so instead i have attempted to delete the thread and recreate it periodically, this works before interference occurs, however after the interference occurs it does manage to create a new thread but it still does not run.
Transmit function:
VOID usbx_cdc_acm_write_thread_entry(ULONG thread_input)
{
/* Private Variables */
ULONG tx_actual_length;
UX_SLAVE_DEVICE *device;
const char ctrStr[10] = "Alive!\n";
device = &_ux_system_slave->ux_system_slave_device;
uint32_t ctr = 0;
char* testData;
while(1)
{
// if ((device->ux_slave_device_state == UX_DEVICE_CONFIGURED) && (cdc_acm != UX_NULL))
// {
//if (tx_queue_receive(&USB_data, &testData, TX_WAIT_FOREVER) == TX_SUCCESS)
// if (tx_queue_receive(&USB_data, &testData, TX_NO_WAIT) == TX_SUCCESS)
// {
// ux_device_class_cdc_acm_write(cdc_acm, testData, strlen(testData), &tx_actual_length);
// }
// else
// {
if (ctr++ > 10)
{
ctr = 0;
ux_device_class_cdc_acm_write(cdc_acm, ctrStr, strlen(ctrStr), &tx_actual_length);
}
tx_thread_sleep(1);
// }
// }
tx_thread_sleep(1);
//free(testData);
}
}
My attempt at solving the problem:
static VOID app_ux_device_thread_entry(ULONG thread_input)
{
int counter = 0;
/*
...
*/
while (1)
{
tx_thread_sleep(100); // <---- Added to allow other processes to run
if(counter > 15){
counter = 0;
UINT status1 = tx_thread_terminate(&ux_cdc_write_thread);
UINT status2 = tx_thread_delete(&ux_cdc_write_thread);
tx_thread_sleep(100);
UINT status3 = tx_thread_create(&ux_cdc_write_thread, "cdc_acm_write_usbx_app_thread_entry", usbx_cdc_acm_write_thread_entry, 1, pointer, 1025, 13, 13, TX_NO_TIME_SLICE, TX_AUTO_START); // Priority was 20
// UINT status4 = tx_thread_resume(&ux_cdc_write_thread);
// int temp = 3;
}
else{
counter++;
}
}
/* USER CODE END app_ux_device_thread_entry */
}