TLSv1.3 in STM32H563 using NetXSecure
Hi
I'm trying to setup TLSv1.3 using STM32H63 Nucleo board. I followed the steps in https://github.com/eclipse-threadx/rtos-docs/blob/main/rtos-docs/netx-duo/netx-duo-secure-tls/chapter3.md to enable TLSv1.3 in STM32CubeMX. But all I get from the OpenSSL server is:
ssl.SSLError: [SSL: NO_SUITABLE_SIGNATURE_ALGORITHM] no suitable signature algorithm (_ssl.c:1006)
How do I solve this? I checked with the debugger and I can see that this code gets hit
#if (NX_SECURE_TLS_TLS_1_3_ENABLED)
if(tls_session->nx_secure_tls_1_3)
{
/* Send supported TLS versions extensions (for TLS 1.3). */
status = _nx_secure_tls_send_clienthello_supported_versions_extension(tls_session, packet_buffer, &length, &extension_length, available_size);
if(status != NX_SUCCESS)
{
return(status);
}
Using wireshark I can see that clienthello from the client
Frame 243: 250 bytes on wire (2000 bits), 250 bytes captured (2000 bits) on interface \Device\NPF_{0B831098-E396-4CE0-B06D-0E743D48CD98}, id 0
Section number: 1
Interface id: 0 (\Device\NPF_{0B831098-E396-4CE0-B06D-0E743D48CD98})
Interface name: \Device\NPF_{0B831098-E396-4CE0-B06D-0E743D48CD98}
Interface description: Ethernet 2
Encapsulation type: Ethernet (1)
Arrival Time: Sep 18, 2024 16:19:29.214045000 W. Europe Daylight Time
UTC Arrival Time: Sep 18, 2024 14:19:29.214045000 UTC
Epoch Arrival Time: 1726669169.214045000
[Time shift for this packet: 0.000000000 seconds]
[Time delta from previous captured frame: 0.311093000 seconds]
[Time delta from previous displayed frame: 19.498310000 seconds]
[Time since reference or first frame: 57.311405000 seconds]
Frame Number: 243
Frame Length: 250 bytes (2000 bits)
Capture Length: 250 bytes (2000 bits)
[Frame is marked: False]
[Frame is ignored: False]
[Protocols in frame: eth:ethertype:ip:tcp:tls]
[Coloring Rule Name: TCP]
[Coloring Rule String: tcp]
Ethernet II, Src: STMicroelect_00:00:00 (00:80:e1:00:00:00), Dst: LuxsharePrec_b9:e4:e6 (60:6d:3c:b9:e4:e6)
Destination: LuxsharePrec_b9:e4:e6 (60:6d:3c:b9:e4:e6)
Address: LuxsharePrec_b9:e4:e6 (60:6d:3c:b9:e4:e6)
.... ..0. .... .... .... .... = LG bit: Globally unique address (factory default)
.... ...0 .... .... .... .... = IG bit: Individual address (unicast)
Source: STMicroelect_00:00:00 (00:80:e1:00:00:00)
Address: STMicroelect_00:00:00 (00:80:e1:00:00:00)
.... ..0. .... .... .... .... = LG bit: Globally unique address (factory default)
.... ...0 .... .... .... .... = IG bit: Individual address (unicast)
Type: IPv4 (0x0800)
Internet Protocol Version 4, Src: 192.168.1.5, Dst: 192.168.1.10
0100 .... = Version: 4
.... 0101 = Header Length: 20 bytes (5)
Differentiated Services Field: 0x00 (DSCP: CS0, ECN: Not-ECT)
0000 00.. = Differentiated Services Codepoint: Default (0)
.... ..00 = Explicit Congestion Notification: Not ECN-Capable Transport (0)
Total Length: 236
Identification: 0x0003 (3)
000. .... = Flags: 0x0
0... .... = Reserved bit: Not set
.0.. .... = Don't fragment: Not set
..0. .... = More fragments: Not set
...0 0000 0000 0000 = Fragment Offset: 0
Time to Live: 128
Protocol: TCP (6)
Header Checksum: 0xb6a9 [validation disabled]
[Header checksum status: Unverified]
Source Address: 192.168.1.5
Destination Address: 192.168.1.10
Transmission Control Protocol, Src Port: 62509, Dst Port: 6000, Seq: 1, Ack: 1, Len: 196
Source Port: 62509
Destination Port: 6000
[Stream index: 1]
[Conversation completeness: Complete, WITH_DATA (31)]
..0. .... = RST: Absent
...1 .... = FIN: Present
.... 1... = Data: Present
.... .1.. = ACK: Present
.... ..1. = SYN-ACK: Present
.... ...1 = SYN: Present
[Completeness Flags: ·FDASS]
[TCP Segment Len: 196]
Sequence Number: 1 (relative sequence number)
Sequence Number (raw): 3489658439
[Next Sequence Number: 197 (relative sequence number)]
Acknowledgment Number: 1 (relative ack number)
Acknowledgment number (raw): 3945295425
0101 .... = Header Length: 20 bytes (5)
Flags: 0x018 (PSH, ACK)
000. .... .... = Reserved: Not set
...0 .... .... = Accurate ECN: Not set
.... 0... .... = Congestion Window Reduced: Not set
.... .0.. .... = ECN-Echo: Not set
.... ..0. .... = Urgent: Not set
.... ...1 .... = Acknowledgment: Set
.... .... 1... = Push: Set
.... .... .0.. = Reset: Not set
.... .... ..0. = Syn: Not set
.... .... ...0 = Fin: Not set
[TCP Flags: ·······AP···]
Window: 8192
[Calculated window size: 8192]
[Window size scaling factor: -2 (no window scaling used)]
Checksum: 0xb067 [unverified]
[Checksum Status: Unverified]
Urgent Pointer: 0
[Timestamps]
[Time since first frame in this TCP stream: 0.451453000 seconds]
[Time since previous frame in this TCP stream: 0.450463000 seconds]
[SEQ/ACK analysis]
[iRTT: 0.000990000 seconds]
[Bytes in flight: 196]
[Bytes sent since last PSH flag: 196]
TCP payload (196 bytes)
Transport Layer Security
TLSv1.2 Record Layer: Handshake Protocol: Client Hello
Content Type: Handshake (22)
Version: TLS 1.2 (0x0303)
Length: 191
Handshake Protocol: Client Hello
Handshake Type: Client Hello (1)
Length: 187
Version: TLS 1.2 (0x0303)
Random: 000000005905b56d8d7d157d43eddf717b97cb45bebba36e904b983a16976d66
GMT Unix Time: Jan 1, 1970 01:00:00.000000000 W. Europe Standard Time
Random Bytes: 5905b56d8d7d157d43eddf717b97cb45bebba36e904b983a16976d66
Session ID Length: 0
Cipher Suites Length: 24
Cipher Suites (12 suites)
Cipher Suite: TLS_AES_128_GCM_SHA256 (0x1301)
Cipher Suite: TLS_AES_128_CCM_SHA256 (0x1304)
Cipher Suite: TLS_AES_128_CCM_8_SHA256 (0x1305)
Cipher Suite: TLS_ECDHE_ECDSA_WITH_AES_128_GCM_SHA256 (0xc02b)
Cipher Suite: TLS_ECDHE_RSA_WITH_AES_128_GCM_SHA256 (0xc02f)
Cipher Suite: TLS_ECDHE_ECDSA_WITH_AES_128_CBC_SHA256 (0xc023)
Cipher Suite: TLS_ECDHE_RSA_WITH_AES_128_CBC_SHA256 (0xc027)
Cipher Suite: TLS_RSA_WITH_AES_128_GCM_SHA256 (0x009c)
Cipher Suite: TLS_RSA_WITH_AES_256_CBC_SHA256 (0x003d)
Cipher Suite: TLS_RSA_WITH_AES_128_CBC_SHA256 (0x003c)
Cipher Suite: TLS_PSK_WITH_AES_128_CBC_SHA256 (0x00ae)
Cipher Suite: TLS_PSK_WITH_AES_128_CCM_8 (0xc0a8)
Compression Methods Length: 1
Compression Methods (1 method)
Compression Method: null (0)
Extensions Length: 122
Extension: supported_groups (len=8)
Type: supported_groups (10)
Length: 8
Supported Groups List Length: 6
Supported Groups (3 groups)
Supported Group: secp256r1 (0x0017)
Supported Group: secp384r1 (0x0018)
Supported Group: secp521r1 (0x0019)
Extension: ec_point_formats (len=2)
Type: ec_point_formats (11)
Length: 2
EC point formats Length: 1
Elliptic curves point formats (1)
EC point format: uncompressed (0)
Extension: supported_versions (len=5) TLS 1.3, TLS 1.2
Type: supported_versions (43)
Length: 5
Supported Versions length: 4
Supported Version: TLS 1.3 (0x0304)
Supported Version: TLS 1.2 (0x0303)
Extension: key_share (len=71) secp256r1
Type: key_share (51)
Length: 71
Key Share extension
Client Key Share Length: 69
Key Share Entry: Group: secp256r1, Key Exchange length: 65
Group: secp256r1 (23)
Key Exchange Length: 65
Key Exchange: 0429c78232b89a29e36d68aa3b422b7847e7b85b95fb955f3b2eb30b321d87e595520b4cb05c57baedd8b42b16bc1ed8240f27d3149448feba1f8979ba47051fe5
Extension: signature_algorithms (len=16)
Type: signature_algorithms (13)
Length: 16
Signature Hash Algorithms Length: 14
Signature Hash Algorithms (7 algorithms)
Signature Algorithm: ecdsa_secp256r1_sha256 (0x0403)
Signature Hash Algorithm Hash: SHA256 (4)
Signature Hash Algorithm Signature: ECDSA (3)
Signature Algorithm: ecdsa_secp384r1_sha384 (0x0503)
Signature Hash Algorithm Hash: SHA384 (5)
Signature Hash Algorithm Signature: ECDSA (3)
Signature Algorithm: ecdsa_secp521r1_sha512 (0x0603)
Signature Hash Algorithm Hash: SHA512 (6)
Signature Hash Algorithm Signature: ECDSA (3)
Signature Algorithm: rsa_pkcs1_sha256 (0x0401)
Signature Hash Algorithm Hash: SHA256 (4)
Signature Hash Algorithm Signature: RSA (1)
Signature Algorithm: rsa_pkcs1_sha384 (0x0501)
Signature Hash Algorithm Hash: SHA384 (5)
Signature Hash Algorithm Signature: RSA (1)
Signature Algorithm: rsa_pkcs1_sha512 (0x0601)
Signature Hash Algorithm Hash: SHA512 (6)
Signature Hash Algorithm Signature: RSA (1)
Signature Algorithm: SHA224 ECDSA (0x0303)
Signature Hash Algorithm Hash: SHA224 (3)
Signature Hash Algorithm Signature: ECDSA (3)
[JA4: t13i120500_300ad538f728_2ddaf29219d6]
[JA4_r: t13i120500_003c,003d,009c,00ae,1301,1304,1305,c023,c027,c02b,c02f,c0a8_000a,000b,000d,002b,0033_0403,0503,0603,0401,0501,0601,0303]
[JA3 Fullstring: 771,4865-4868-4869-49195-49199-49187-49191-156-61-60-174-49320,10-11-43-51-13,23-24-25,0]
[JA3: 0fe05bb12fd3c7ca77de173a4deb6eae]
which results in a handshake failure
Ethernet II, Src: LuxsharePrec_b9:e4:e6 (60:6d:3c:b9:e4:e6), Dst: STMicroelect_00:00:00 (00:80:e1:00:00:00) Destination: STMicroelect_00:00:00 (00:80:e1:00:00:00) Address: STMicroelect_00:00:00 (00:80:e1:00:00:00) .... ..0. .... .... .... .... = LG bit: Globally unique address (factory default) .... ...0 .... .... .... .... = IG bit: Individual address (unicast) Source: LuxsharePrec_b9:e4:e6 (60:6d:3c:b9:e4:e6) Address: LuxsharePrec_b9:e4:e6 (60:6d:3c:b9:e4:e6) .... ..0. .... .... .... .... = LG bit: Globally unique address (factory default) .... ...0 .... .... .... .... = IG bit: Individual address (unicast) Type: IPv4 (0x0800) Internet Protocol Version 4, Src: 192.168.1.10, Dst: 192.168.1.5 0100 .... = Version: 4 .... 0101 = Header Length: 20 bytes (5) Differentiated Services Field: 0x00 (DSCP: CS0, ECN: Not-ECT) 0000 00.. = Differentiated Services Codepoint: Default (0) .... ..00 = Explicit Congestion Notification: Not ECN-Capable Transport (0) Total Length: 47 Identification: 0xdb69 (56169) 010. .... = Flags: 0x2, Don't fragment 0... .... = Reserved bit: Not set .1.. .... = Don't fragment: Set ..0. .... = More fragments: Not set ...0 0000 0000 0000 = Fragment Offset: 0 Time to Live: 128 Protocol: TCP (6) Header Checksum: 0x0000 [validation disabled] [Header checksum status: Unverified] Source Address: 192.168.1.10 Destination Address: 192.168.1.5 Transmission Control Protocol, Src Port: 6000, Dst Port: 62509, Seq: 1, Ack: 197, Len: 7 Source Port: 6000 Destination Port: 62509 [Stream index: 1] [Conversation completeness: Complete, WITH_DATA (31)] ..0. .... = RST: Absent ...1 .... = FIN: Present .... 1... = Data: Present .... .1.. = ACK: Present .... ..1. = SYN-ACK: Present .... ...1 = SYN: Present [Completeness Flags: ·FDASS] [TCP Segment Len: 7] Sequence Number: 1 (relative sequence number) Sequence Number (raw): 3945295425 [Next Sequence Number: 8 (relative sequence number)] Acknowledgment Number: 197 (relative ack number) Acknowledgment number (raw): 3489658635 0101 .... = Header Length: 20 bytes (5) Flags: 0x018 (PSH, ACK) 000. .... .... = Reserved: Not set ...0 .... .... = Accurate ECN: Not set .... 0... .... = Congestion Window Reduced: Not set .... .0.. .... = ECN-Echo: Not set .... ..0. .... = Urgent: Not set .... ...1 .... = Acknowledgment: Set .... .... 1... = Push: Set .... .... .0.. = Reset: Not set .... .... ..0. = Syn: Not set .... .... ...0 = Fin: Not set [TCP Flags: ·······AP···] Window: 64044 [Calculated window size: 64044] [Window size scaling factor: -2 (no window scaling used)] Checksum: 0x8381 [unverified] [Checksum Status: Unverified] Urgent Pointer: 0 [Timestamps] [Time since first frame in this TCP stream: 0.451832000 seconds] [Time since previous frame in this TCP stream: 0.000379000 seconds] [SEQ/ACK analysis] [This is an ACK to the segment in frame: 243] [The RTT to ACK the segment was: 0.000379000 seconds] [iRTT: 0.000990000 seconds] [Bytes in flight: 7] [Bytes sent since last PSH flag: 7] TCP payload (7 bytes) Transport Layer Security TLSv1.2 Record Layer: Alert (Level: Fatal, Description: Handshake Failure) Content Type: Alert (21) Version: TLS 1.2 (0x0303) Length: 2 Alert Message Level: Fatal (2) Description: Handshake Failure (40)
Am I missing some extra configuration? Any tips would be helpful