UART bootloader in the Nucleo-L476RG - Getting NACK from the beginning
Hi,
I wanted to use the bootloader via uart in a nucleo-L476RG (target) and have an L4P5ZG as a Master. I read the AN2606 and AN3155 but I am facing some problems.
The activation pattern is the 7. I did the following:
- BOOT0->to VDD
- nBoot1 ->1
-BFB2->0 ( default value)
I connected the TX-RX and The RX-TX and the GND of both boards. I am using USART_1 ( I tried normal uart before and it seems to work) in both.
I used the USB to power them.
In the c code, I sent the first 0x7F.
But I am always receiving a NACK(0x1F), so I cannot continue with the commands ( I wanted to send the get command to see if it was working before doing anything else).
I am doing something wrong obviously but I do not know what, I read the application notes but I do not know what I am missing.
Do you have any idea?
I am not doing anything with the reset, can this be related? In some forums, they mention the reset but in the application note, it does not say much about this so I do not know what to do exactly with it. And I am getting some response from the bootloader tho.
If you know a host example code in c, that uses uart to access the bootloader it would be great to check.
Thank you in advance.