Skip to main content
Visitor II
June 21, 2021
Question

UART Bootloder protocol: Write command have no effect on memory, despite all required ACKs recieved.

  • June 21, 2021
  • 4 replies
  • 1751 views

Hi, i have problem with bootloader protocol on USART. Write command gives all ACKs but there is no effect on memory.

Other commands seems to work fine, with all ACKs, i can read memory fine. I was checking memory using STM Programmer.

I'm using NUCLEO F439ZI.

Termios settings for UART are:

cfmakeraw(&settings);

settings.c_cflag &= ~PARODD;

settings.c_cflag |= PARENB;

settings.c_cflag &= ~CSTOPB;

settings.c_cc[VMIN] = 0;

settings.c_cc[VTIME] = 10;

cfsetispeed(&settings, B115200);

cfsetospeed(&settings, B115200);

Commands used for tests are:

printf "\x7F\x31\xCE" >/dev/ttymxc2

printf "\x08\x00\x00\x00\x08" >/dev/ttymxc2

printf "\x03\x55\x55\x55\x55\x03" >/dev/ttymxc2

For those commands i receive 4 ACKs.

Then using :

 printf "\x7F\x11\xEE" >/dev/ttymxc2

 printf "\x08\x00\x00\x00\x08" >/dev/ttymxc2

 printf "\x0F\xF0" >/dev/ttymxc2

Gives unchanged memory back.

    This topic has been closed for replies.

    4 replies

    Super User
    June 21, 2021

    0x7F is only used once to start bootloader mode. You shouldn't be using it between each command. I would expect stray 0x7Fs to cause a NACK.

    You should probably wait between the very first 0x7F and the first command sent to allow the chip time to enter UART bootloader mode, although it might not be needed.

    If that's not it, not sure. I've used the UART bootloader on the STM32F4 extensively.

    Super User
    June 21, 2021

    You are erasing the flash before writing to it, correct? What values do you receive back? Flash bits can only go from 1 to 0 when writing.

    MBrze.2Author
    Visitor II
    June 22, 2021

    No, i'm not erasing the flash. Does every write require clearing whole flash before that?

    I'm using 0x7F only one time, between resetting device into bootmode.

    The problem is i don't get NACKs.

    Super User
    June 22, 2021

    If you want to change bits from 0 to 1, you need to erase the flash page.

    You didn't answer my question about what values you receive back.

    MBrze.2Author
    Visitor II
    June 22, 2021

    I only get ACKs back.

    If you mean what i get back when i read from memory, then i receive the same memory that there was. (checked using STMprogrammer)

    MBrze.2Author
    Visitor II
    June 22, 2021

    Well, it was something random, data there is lost now.

    Sorry, i didn't reply.