UART_DMARxHalfCplt is bugged for STM32G0
In the stm32g0xx_hal_uart.c file, line 3750 the following function can be found:
/**
* @brief DMA UART receive process half complete callback.
* @param hdma DMA handle.
* @retval None
*/
static void UART_DMARxHalfCplt(DMA_HandleTypeDef *hdma)
{
UART_HandleTypeDef *huart = (UART_HandleTypeDef *)(hdma->Parent);
/* Check current reception Mode :
If Reception till IDLE event has been selected : use Rx Event callback */
if (huart->ReceptionType == HAL_UART_RECEPTION_TOIDLE)
{
#if (USE_HAL_UART_REGISTER_CALLBACKS == 1)
/*Call registered Rx Event callback*/
huart->RxEventCallback(huart, huart->RxXferSize/2U);
#else
/*Call legacy weak Rx Event callback*/
HAL_UARTEx_RxEventCallback(huart, huart->RxXferSize/2U);
#endif /* USE_HAL_UART_REGISTER_CALLBACKS */
}
else
{
/* In other cases : use Rx Half Complete callback */
#if (USE_HAL_UART_REGISTER_CALLBACKS == 1)
/*Call registered Rx Half complete callback*/
huart->RxHalfCpltCallback(huart);
#else
/*Call legacy weak Rx Half complete callback*/
HAL_UART_RxHalfCpltCallback(huart);
#endif /* USE_HAL_UART_REGISTER_CALLBACKS */
}
}It can be noticed that in case the reception mode is set to HAL_UART_RECEPTION_TOIDLE, an incorrect callback function is called (huart->RxEventCallback or HAL_UARTEx_RxEventCallback). The library lacks a dedicated "idle half rx callback" function. Because of this, the reception callback is called twice if the amount of received data exceeds half of the buffer size.
@Imen DAHMEN can you please confirm?