UART Interrupt problem with STM32L412KB
I am encountering an issue with UART receiving interrupt, where it intermittently stops receiving data after a series of AT commands have been sent to a GSM modem. The UART communication is configured to use DMA for data transfer, and we have assigned the appropriate DMA channels.
Following is the code: On initialization:
MX_USART1_UART_Init(); //UART Initialization
HAL_UARTEx_ReceiveToIdle_DMA(&huart1, RX_Buffer1, 50); //Enable Interrupt
The below is the code for transmitting AT commands:
memset(RX_Buffer1,0,sizeof(RX_Buffer1)); //Clearing the receive buffer
memset(ATcommand,0,sizeof(ATcommand)); // clearing the transmit buffer
sprintf(ATcommand,transmit_commands[AT_command_number]); //Get command from the command array
HAL_UART_Transmit(&huart1,(uint8_t *)ATcommand,strlen(ATcommand),1000); // UART Transmit
HAL_Delay(300); ///Delay 300 msec
The issue manifests as the UART interrupt ceasing to function properly after sending a certain number of AT commands. The interrupt is designed to process the responses received from the GSM modem and trigger further actions based on those responses. However, after executing the "AT+CCLK?" command for the second time, the interrupt stops functioning.
Restarting the device by deinitializing and initializing the UART resolves the problem temporarily. However, this is not a practical solution, as we cannot reset the UART after every transmit operation.
Kindly refer to the provided log that details the sequence of AT commands transmitted and the accompanying responses received. Within this log, you can observe a noticeable interruption in the functioning of the UART interrupt, which seems to be the core of the problem.
Any insights, guidance, or solutions from the community would be greatly appreciated.