UART Synchronisation issue LCM GUI display for NUCLEO-h743zi2 board
Dear Team,
I am interfacing Nucleo-h743zi2 board with LCM display(GUI) through UART using Interrupt method.
I can transmit the data to LCM and it is displaying properly on the LCM display.
Now I am trying to send the commands from LCM display to STM controller.
I tried to press the button for many times on LCM display and observed sometimes it is triggering and sometimes not triggered). I think there is a problem with synchronisation for receiving from LCM display to STM controller. I can see the events are triggered sometimes in debugging steps.
I tried to change the system clock to different values but it did not worked. Also I tried to increase the delays, decreasing delays at different places did not worked.
I tried to copy the receiving buffer into the other buffer and cleared the buffer. But this also does not worked.
Please find the below Receive function for your reference:
extern uint8_t data_u[100];
uint8 j, max;
It is mentioned in LCM document as follows:
your serial receive function should timeout after 0.1s (= SERIAL_ATOMIC_TIMEOUT defined in "config.master.h").
All other timeouts must be multiples of this (see "config.master.h" again):
#define SERIAL_ATOMIC_TIMEOUT 1 /*!< in tenth of seconds (default 0.1s); the
timeout of the serial port should be
configured to the same time (0.1s) */
#define SERIAL_NORMAL_TIMEOUT 20 /*!< in tenth of seconds (default 2s), must
be a multiple of the
SERIAL_ATOMIC_TIMEOUT */
#define SERIAL_FLASH_TIMEOUT 600 /*!< in tenth of seconds (default 60s), must
be a multiple of the
SERIAL_ATOMIC_TIMEOUT */
For every "normal" command you should receive a response package after 2s (= SERIAL_NORMAL_TIMEOUT).
You have to wait for the response befor sending the next command.
Please guide me to know how we can resolve the synchronisation issues by using above LCM information .
Do I need to use timer for 0.1sec to receive function. If yes could you please help me to know how we can write it in code.