Unable to get RAM Disk as USB MSD for mbed & Nucleo-F401-RE
Hi,
I am new to mbed and STM32-F401RE.
I am trying to get the RAM Disk as USB Mass storage device and communicate between PC and STM board. I am trying https://os.mbed.com/users/va009039/code/F401RE_USBMSD_RAM/
I am able to run the binary but board is not detected as USB Drive on the Windows.
- define PACKET_SIZE 32
- define blocks_data (1024 * 512)
FATFileSystem fs("fs");
SERIAL setup Serial pc(USBTX, USBRX, 230400);
THREADs Thread ramfs_thread;
void ram_disk_setup() { int connect1 = 0;
/* Size of RAM file system exposed to PC as USB MassStorage */ HeapBlockDevice heap_bd(blocks_data, 512);
MBRBlockDevice::partition(&heap_bd, 1, 0x0b, 0, 512 * 512);
MBRBlockDevice part1(&heap_bd, 1);
RAMFS ramfs1("ram1", &part1);
format with FS FATFileSystem::format(&part1); create FS object and mount FS FATFileSystem fat1("fat", &part1);
USBRAMFS usbmsd1(&ramfs1);
now we wait for the user to connect the board to the PC while(true) { if (usbmsd1.connect() && 1 != connect1) { connect1 = 1; printf("Connected to PC - 1\r\n"); }
only try once per second Thread::wait(9000); } }
int main(void) { osStatus err; wait(5);
printf("\r\nUSB Serial done\r\n");
err = ramfs_thread.start(callback(ram_disk_setup)); if (err) { printf("ERROR > send_hid_thread not created\r\n"); } ramfs_thread.join(); }
Thank you in advance.
Regards,
Jignesh